imx6q: building linux image with both fb & x11 backends

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q: building linux image with both fb & x11 backends

917 Views
pj0585
Contributor III

Hi,

I want to build the latest fsl-community-bsp image

(fsl-L3.14.28_1.0.0_ga). I can choose to build any one backend (fb, x11,

wayland or directfb). The libraries of the other backends are removed

or not built.

Is it possible to build the image for framebuffer (fb) backend but

also include libraries of the x11 backend ? If yes, can someone please point out to me how can I do this?

Regards, Pj

Labels (4)
0 Kudos
Reply
0 Replies