imx6q build LTIB problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q build LTIB problems

Jump to solution
1,440 Views
ivychend
Contributor I

I have downloaded source code "L3.0.35_4.1.0_130816_source.tar.gz" from official website. and build compiled environment in ubuntu 12.04 followed the document. when I compiled the source code, I got an error "make: *** No rule to make target `mx6q_sabresd_config'.  Stop."  I tried again and again to build environment and compile from scratch, but the error were still there. I searched information related, but faild to find any. I want to know how to solve this problem, do I miss some steps??

Labels (2)
0 Kudos
Reply
1 Solution
1,169 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  In addition to recommendations of the following document, please pay attention on the

recent recommendations regarding host PC setup in "Setting_up_LTIB_Host.pdf", section 1.11

(Special for Ubuntu 11.10) from the Linux documentation.

 

https://community.nxp.com/servlet/JiveServlet/download/271839-220893/438-CreateUbuntu1110ltib110901.... 

 

Also, the following may help.

Using i.MX 6 Series LTIB on Host Ubuntu 14.04 Trusty Tahr  

 

Documentation may be found at http://www.nxp.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,170 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  In addition to recommendations of the following document, please pay attention on the

recent recommendations regarding host PC setup in "Setting_up_LTIB_Host.pdf", section 1.11

(Special for Ubuntu 11.10) from the Linux documentation.

 

https://community.nxp.com/servlet/JiveServlet/download/271839-220893/438-CreateUbuntu1110ltib110901.... 

 

Also, the following may help.

Using i.MX 6 Series LTIB on Host Ubuntu 14.04 Trusty Tahr  

 

Documentation may be found at http://www.nxp.com/webapp/Download?colCode=L3.0.35_4.1.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 Kudos
Reply