on my custom im6q board, run m6.0.1_2.1.0-ga boot from TF card (in SDHC2 slot, 64GB), flash tool is ./device/fsl/common/tools/fsl-sdcard-partition.sh,
system stuck at keep scaning the "android" logo, and i got the error bellow from the boot info:
EXT4-fs (mmcblk1p5): mounted filesystem with ordered data mode. Opts: barrier=1
fs_mgr: __mount(source=/dev/block/mmcblk1p5,target=/system,type=ext4)=0
fs_mgr: __mount(source=/dev/block/mmcblk1p4,target=/data,type=ext4)=-1
fs_mgr: fs_mgr_mount_all(): possibly an encryptable blkdev /dev/block/mmcblk1p4)
fs_mgr: __mount(source=/dev/block/mmcblk1p6,target=/cache,type=ext4)=-1
fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblm
EXT4-fs (mmcblk1p7): mounted filesystem with ordered data mode. Opts: (null)
fs_mgr: __mount(source=/dev/block/mmcblk1p7,target=/device,type=ext4)=0
init: fs_mgr_mount_all returned an error
init: fs_mgr_mount_all returned unexpected error 255
what can i do then? thanks a lot.
attached files are burn-log and boot-log.
Original Attachment has been moved to: burn-log.txt.zip
Original Attachment has been moved to: minicom1930.cap.zip