imx6q android user AP6441(bcm43341 wifi )error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q android user AP6441(bcm43341 wifi )error

4,918 次查看
xiaoliangguan
Contributor I

wifi驱动移植
                               1、在终端通过wireless-tool 可以加载驱动,加载网卡,加载网卡时候有个错误(dhd_preinit_ioctls wl ampdu_hostreorder failed -23)
                               2、在终端可以扫描到周围热点,也可以连接上,通过udhcp -i 可以获取到ip,可以ping 通手机热点。
                               3、在上层,android界面可以看到扫描到热点,也可以连接上(通过打印可以连接上),通过dhcp获取ip也正常。
                               4、android界面一直是获取ip,就断开,然后在
扫描,连接,获取ip,在断开 ,循环 

log 内容包括
         1、驱动的加载的log
         2、网卡启动的log
         3、手动启动dhcp -d 时候的log (底层驱动打印的,上层打印的)
         4、通过界面连接启动时候android上层的打印
1/*********************************************驱动加载log***************************************/
[  107.677860] dhd_module_init: in
[  107.681095] get into function::dhd_wifi_platform_register_drv--->step2
[  107.687758] ======== bcm_wlan_set_plat_data ========
[  107.692786] ------------[ cut here ]------------
[  107.697482] WARNING: at drivers/gpio/gpiolib.c:101 gpio_ensure_requested+0x54/0x1b0()
[  107.705424] autorequest GPIO-185
[  107.708712] Modules linked in: bcmdhd(+)
[  107.712918] [<c009efe4>] (unwind_backtrace+0x0/0x138) from [<c00d793c>] (warn_slowpath_common+0x4c/0x64)
[  107.722520] [<c00d793c>] (warn_slowpath_common+0x4c/0x64) from [<c00d79e8>] (warn_slowpath_fmt+0x30/0x40)
[  107.732157] [<c00d79e8>] (warn_slowpath_fmt+0x30/0x40) from [<c030bce0>] (gpio_ensure_requested+0x54/0x1b0)
[  107.742023] [<c030bce0>] (gpio_ensure_requested+0x54/0x1b0) from [<c030c2a0>](gpio_direction_input+0xa4/0x1fc)
[  107.752418] [<c030c2a0>] (gpio_direction_input+0xa4/0x1fc) from [<bf042740>](bcm_wlan_get_oob_irq+0xc/0x24 [bcmdhd])
[  107.763386] [<bf042740>] (bcm_wlan_get_oob_irq+0xc/0x24 [bcmdhd]) from [<bf014ed0>] (dhd_wifi_platform_register_drv+0x84/0xfc [bcmdhd])
[  107.775878] [<bf014ed0>] (dhd_wifi_platform_register_drv+0x84/0xfc [bcmdhd])from [<bf0a0078>] (dhd_module_init+0x78/0x154 [bcmdhd])
[  107.788022] [<bf0a0078>] (dhd_module_init+0x78/0x154 [bcmdhd]) from [<c0091640>] (do_one_initcall+0xfc/0x164)
[  107.798068] [<c0091640>] (do_one_initcall+0xfc/0x164) from [<c010f95c>] (sys_init_module+0xdc8/0x1c78)
[  107.807504] [<c010f95c>] (sys_init_module+0xdc8/0x1c78) from [<c0097900>] (ret_fast_syscall+0x0/0x30)
[  107.816841] ---[ end trace e4a110f4056e0534 ]---
[  107.821574] host_oob_irq: 441
[  107.824841] host_oob_irq_flags=1044
[  107.828390] dhd_wifi_platform_load: Enter
[  107.832473] get into function dhd_wifi_platform_load !
[  107.837738]  get into function-->dhd_wifi_platform_load_usb !
[  107.843546] get into function dhd_wifi_platform_load_sdio !
[  107.849245] Power-up adapter 'DHD generic adapter'
[  107.854343] wifi_platform_set_power = 1
[  107.858255] ======== PULL WL_REG_ON HIGH! ========
[  107.963072] get into function --->wifi_card_detect
[  108.041738] mmc2: queuing unknown CIS tuple 0x80 (2 bytes)
[  108.049081] mmc2: queuing unknown CIS tuple 0x80 (3 bytes)
[  108.056351] mmc2: queuing unknown CIS tuple 0x80 (3 bytes)
[  108.065044] mmc2: queuing unknown CIS tuple 0x80 (7 bytes)
[  108.140884] mmc2: queuing unknown CIS tuple 0x91 (3 bytes)
[  108.146539] mmc2: new high speed SDIO card at address 0001
[  108.174711] wifi_platform_bus_enumerate device present 1
[  108.180140] ======== Card detection to detect SDIO card! ========
[  108.217639] mmc2: queuing unknown CIS tuple 0x80 (2 bytes)
[  108.224951] mmc2: queuing unknown CIS tuple 0x80 (3 bytes)
[  108.232206] mmc2: queuing unknown CIS tuple 0x80 (3 bytes)
[  108.240887] mmc2: queuing unknown CIS tuple 0x80 (7 bytes)
[  108.286258] get into function --->wifi_card_detect
[  108.329036] bcmsdh_register: register client driver
[  108.397667] mmc2: queuing unknown CIS tuple 0x80 (2 bytes)
[  108.404954] mmc2: queuing unknown CIS tuple 0x80 (3 bytes)
[  108.412294] mmc2: queuing unknown CIS tuple 0x80 (3 bytes)
[  108.420910] mmc2: queuing unknown CIS tuple 0x80 (7 bytes)
[  108.492384] bcmsdh_sdmmc: bcmsdh_sdmmc_probe Enter
[  108.497335] bcmsdh_sdmmc: bcmsdh_sdmmc_probe Enter
[  108.502242] bus num (host idx)=2, slot num (rca)=1
[  108.507109] found adapter info 'DHD generic adapter'
[  108.512569] dhdsdio_probe : no mutex held. set lock
[  108.517650] F1 signature read @0x18000000=0x1602a94d
[  108.525944] F1 signature OK, socitype:0x1 chip:0xa94d rev:0x2 pkg:0x0
[  108.533062] DHD: dongle ram size is set to 524288(orig 524288) at 0x0
[  108.540317] dhd_conf_set_chiprev: chip=0xa94d, chiprev=2
[  108.545761] dhd_conf_set_conf_path_by_nv_path: config_path=/system/etc/firmware/config.txt
[  108.554719] dhd_conf_read_config: Ignore config file /system/etc/firmware/config.txt
[  108.563609] wl_create_event_handler(): thread:wl_event_handler:d55 started
[  108.563618] tsk Enter, tsk = 0xd25013f0
[  108.575964] p2p0: P2P Interface Registered
[  108.581628] dhd_attach(): thread:dhd_watchdog_thread:d5b started
[  108.588378] dhd_attach(): thread:dhd_dpc:d5e started
[  108.588394] dhd_dpc_thread: set dpc_cpucore 0 from config.txt
[  108.599476] dhd_attach(): thread:dhd_rxf:d5f started
[  108.604582] dhd_deferred_work_init: work queue initialized
[  108.610485] dhdsdio_probe_init: set use_rxchain 1 from config.txt
[  108.645319] Dongle Host Driver, version 1.201.59.4 (r506368)
[  108.645327] Compiled in drivers/net/wireless/bcmdhd on Sep  1 2016 at 09:50:17
[  108.659631] Register interface [wlan0]  MAC: 6c:fa:a7:de:81:e0
[  108.672047] dhd_prot_ioctl : bus is down. we have nothing to do
[  108.678324] bcmsdh_oob_intr_unregister: Enter
[  108.684726] bcmsdh_oob_intr_unregister: irq is not registered
[  108.690651] dhd_txglom_enable: enable 0
[  108.694574] dhd_bus_devreset:  WLAN OFF DONE
[  108.699108] wifi_platform_set_power = 0
[  108.703011] ======== PULL WL_REG_ON LOW! ========
[  108.707810] dhdsdio_probe : the lock is released.
[  108.712929] get into function::dhd_wifi_platform_register_drv--->step3
[  108.719544] wifi_ctrlfunc_register_drv--->err =0
[  108.724279] dhd_module_init: Exit err=0

2/**********************************************网卡启动的log*********************************************/
[   69.498661] dhd_open: Enter d6b1b000
[   69.502334]
[   69.502336] Dongle Host Driver, version 1.201.59.4 (r506368)
[   69.502340] Compiled in drivers/net/wireless/bcmdhd on Sep  1 2016 at 09:50:17
[   69.516959] wl_android_wifi_on in 1
[   69.520511] wl_android_wifi_on in 2: g_wifi_on=0
[   69.525198] wifi_platform_set_power = 1
[   69.529095] ======== PULL WL_REG_ON HIGH! ========
[   69.633895] get into function --->wifi_card_detect
[   69.844747] sdio_reset_comm():
[   69.892707] dhd_bus_devreset: == WLAN ON ==
[   69.900232] F1 signature read @0x18000000=0x1602a94d
[   69.909414] F1 signature OK, socitype:0x1 chip:0xa94d rev:0x2 pkg:0x0
[   69.916586] DHD: dongle ram size is set to 524288(orig 524288) at 0x0
[   69.923970] dhdsdio_probe_init: set use_rxchain 1 from config.txt
[   69.930231] dhd_conf_read_config: Ignore config file /system/etc/firmware/config.txt
[   69.938112] dhd_conf_set_fw_name_by_chip: firmware_path=/system/etc/firmware/fw_bcm43341b0_ag.bin
[   69.947118] Final fw_path=/system/etc/firmware/fw_bcm43341b0_ag.bin
[   69.953449] Final nv_path=/system/etc/firmware/nvram.txt
[   69.958887] Final conf_path=/system/etc/firmware/config.txt
[   70.022906] NVRAM version: AP6441_NVRAM_V1.1_20131224
[   70.030766] dhdsdio_write_vars: Download, Upload and compare of NVRAM succeeded.
[   70.197179] dhd_bus_init: enable 0x06, ready 0x06 (waited 0us)
[   70.203398] bcmsdh_oob_intr_register: Enter
[   70.207668] bcmsdh_oob_intr_register: HW_OOB enabled
[   70.212750] bcmsdh_oob_intr_register OOB irq=319 flags=414
[   70.218338] bcmsdh_oob_intr_register: enable_irq_wake
[   70.223454] add wake up source irq 101
[   70.229155] dhd_conf_set_band: Set band 0
[   70.235568] Firmware up: op_mode=0x0015, MAC=6c:fa:a7:de:81:e0
[   70.241520] dhd_conf_set_country: Set country CN, revision 0
[   70.320133] Country code: CN (CN/0)
[   70.324031] dhd_conf_set_roam: Set roam_off 1
[   70.338491] Firmware version = wl0: Jan 20 2014 11:06:06 version 6.10.190.43(r449836) FWID 01-77015d04
[   70.348040]   Driver: 1.201.59.4 (r506368)
[   70.348045]   Firmware: wl0: Jan 20 2014 11:06:06 version 6.10.190.43 (r449836) FWID 01-77015d04
[   70.361528] dhd_txglom_enable: enable 0
[   70.365461] dhd_conf_set_disable_proptx: set disable_proptx 0
[   70.377979] dhd_preinit_ioctls wl ampdu_hostreorder failed -23   (这个错误是什么意思,或者有什么引起的,可以忽略吗)                  
[   70.384405] wl_android_wifi_on: Success
[   70.389082] p2p0: p2p_dev_addr=6e:fa:a7:de:81:e0
[   70.418972] dhd_open: Exit ret=0
[   81.254753] wlan0: no IPv6 routers present

3/****************************************dhcp -d  启动的log**********************************************/
     /******************************************底层的打印************************************************/
  205.827209] Connectting with 6c:fa:a7:de:81:cb channel (2) ssid "QYAP-V2-23456-m2 note-fd", len (24)
[  205.935793] wl_iw_event: Link UP with BSSID=6c:fa:a7:de:81:cb
[  205.942046] wl_bss_connect_done succeeded with 6c:fa:a7:de:81:cb
[  206.066152] dhd_pno_get_for_batch : wifi location service is not supported
[  206.073382] CFG80211-ERROR) wl_is_linkdown :
[  206.077726] ANDROID-ERROR) failed to getting batching results
[  206.083883] Link down Reason : WLC_E_DEAUTH_IND
[  206.088643] link down if eth1 may call cfg80211_disconnected. event : 6, reason=3 from 6c:fa:a7:de:81:cb
[  206.090870] dhd_pno_stop_for_batch : wifi location service is not supported           
[  206.090880] NULL POINTER (_dhd_pno_clear_all_batch_results) : head->next is NULL
[  206.090887] NULL POINTER (_dhd_pno_clear_all_batch_results) : head->next is NULL
[  206.090893] ANDROID-ERROR) failed to stop batching scan
[  206.127908] wl_iw_event: Link Down with BSSID=6c:fa:a7:de:81:cb
[  206.134411] CFG80211-ERROR) wl_is_linkdown : Link down Reason : WLC_E_LINK
[  206.143106] cfg80211: Calling CRDA to update world regulatory domain
[  206.904686] p2p0: no IPv6 routers present
[  207.704866] Connectting with 6c:fa:a7:de:81:cb channel (2) ssid "QYAP-V2-23456-m2 note-fd", len (24)
[  208.695265] connect failed event=0 e->status 3 e->reason 0
[  208.704249] CFG80211-ERROR) wl_bss_connect_done : Report connect result - connection failed
    /******************************************底层的打印************************************************/
    /******************************************通过adb 打印出来***************************************/
    1|root@sabresd_6dq:/ # dhcpcd -d eth1
dhcpcd[5990]: version 5.5.6 starting
dhcpcd[5990]: eth1: using hwaddr 6c:fa:a7:de:81:cb
dhcpcd[5990]: eth1: executing `/system/etc/dhcpcd/dhcpcd-run-hooks', reason PREINIT
dhcpcd[5990]: eth1: executing `/system/etc/dhcpcd/dhcpcd-run-hooks', reason CARRIER
dhcpcd[5990]: eth1: reading lease `/data/misc/dhcp/dhcpcd-eth1.lease'
dhcpcd[5990]: eth1: rebinding lease of 192.168.31.223
dhcpcd[5990]: eth1: sending REQUEST (xid 0xb954b3ee), next in 3.47 seconds
dhcpcd[5990]: eth1: acknowledged 192.168.31.223 from 192.168.31.1
dhcpcd[5990]: eth1: checking for 192.168.31.223
dhcpcd[5990]: eth1: sending ARP probe (1 of 3), next in 1.76 seconds
dhcpcd[5990]: eth1: sending ARP probe (2 of 3), next in 1.75 seconds
dhcpcd[5990]: eth1: sending ARP probe (3 of 3), next in 2.00 seconds
dhcpcd[5990]: eth1: leased 192.168.31.223 for 43200 seconds
dhcpcd[5990]: eth1: adding IP address 192.168.31.223/24
dhcpcd[5990]: eth1: adding route to 192.168.31.0/24
dhcpcd[5990]: eth1: adding default route via 192.168.31.1
dhcpcd[5990]: eth1: writing lease `/data/misc/dhcp/dhcpcd-eth1.lease'
dhcpcd[5990]: eth1: executing `/system/etc/dhcpcd/dhcpcd-run-hooks', reason BOUND
dhcpcd[5990]: forking to background
dhcpcd[5990]: forked to background, child pid 6029

  /******************************************通过adb 打印出来***************************************/
 /****************************************dhcp -d  启动的log**********************************************/


4/******************************************通过界面连接启动时候android上层的打印***************************************/
/wpa_supplicant( 3390): eth1: Associated with 28:6c:07:56:f9:25

D/Ethernet( 2642): Interface eth1 link up

D/Ethernet( 2642): Interface eth1 link up

D/Ethernet( 2642): Interface eth1 link up

D/Ethernet( 2642): Interface eth1 link up

D/Ethernet( 2642): Interface eth1 link up

I/wpa_supplicant( 3390): eth1: WPA: Key negotiation completed with 28:6c:07:56:f9:25 [PTK=CCMP GTK=TKIP]

I/wpa_supplicant( 3390): eth1: CTRL-EVENT-CONNECTED - Connection to 28:6c:07:56:f9:25 completed (auth) [id=0 id_str=]

D/Ethernet( 2642): Interface eth1 link up

E/wpa_supplicant( 3390): wpa_driver_nl80211_driver_cmd: failed to issue private commands

E/WifiStateMachine( 2642): Unexpected BatchedScanResults :null

E/wpa_supplicant( 3390): wpa_driver_nl80211_driver_cmd: failed to issue private commands

I/wpa_supplicant( 3390): eth1: WPA: Key negotiation completed with 28:6c:07:56:f9:25 [PTK=CCMP GTK=TKIP]
D/WifiStateMachine( 2642): VerifyingLinkState enter

D/WifiStateMachine( 2642): VerifyingLinkState GOOD_LINK_DETECTED: transition to captive portal check

D/WifiStateMachine( 2642): CaptivePortalCheckState enter

D/WifiStateMachine( 2642): CaptivePortalCheckState CMD_CAPTIVE_CHECK_COMPLETE

D/ConnectivityService( 2642): Captive portal check NetworkInfo: type: WIFI[], state: CONNECTING/CAPTIVE_PORTAL_CHECK, reason: (unspecified), extra: "lovensMIWIFI", roaming: false, failover: false, isAvailable: true, isConnectedToProvisioningNetwork: false

D/ConnectivityService( 2642): handleCaptivePortalTrackerCheck: call captivePortalCheckComplete ni=NetworkInfo: type: WIFI[], state: CONNECTING/CAPTIVE_PORTAL_CHECK, reason: (unspecified), extra: "lovensMIWIFI", roaming: false, failover: false, isAvailable: true, isConnectedToProvisioningNetwork: false

D/ConnectivityService( 2642): ConnectivityChange for WIFI: CONNECTED/CONNECTED

E/ConnectivityService( 2642): Unexpected mtu value: android.net.wifi.WifiStateTracker@41965b70

D/Nat464Xlat( 2642): requiresClat: netType=1, hasIPv4Address=true

D/ConnectivityService( 2642): ConnectivityChange for ETHERNET: CONNECTED/CONNECTED

D/ConnectivityService( 2642): Policy requires WIFI teardown
I/wpa_supplicant( 3390): eth1: CTRL-EVENT-DISCONNECTED bssid=28:6c:07:56:f9:25 reason=3 locally_generated=1

E/ConnectivityService( 2642): Unexpected mtu value: android.net.EthernetDataTracker@41ae41d0

D/Ethernet( 2642): Interface eth1 link up

D/NetUtils( 2642): dhcp_do_request failed : eth1 (new)

E/Ethernet( 2642): DHCP request error:Timed out waiting for DHCP to finish
/******************************************通过界面连接启动时候android上层的打印***************************************/

大家知道这是什么原因造成的?谢谢!

标签 (1)
0 项奖励
回复
2 回复数

4,126 次查看
igorpadykov
NXP Employee
NXP Employee

Hi  xiaoliang

for porting driver you may wish to request direct support from vendor

wireless.murata.com/eng/products/rf-modules-1/wi-fi-bluetooth-for-freescale-i-mx.html

Best regards
igor

0 项奖励
回复

4,126 次查看
karltsou
Contributor I

Hi,

What's your kernel version?

0 项奖励
回复