i.MX6Q TZASC Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q TZASC Interrupt

Jump to solution
2,714 Views
vsiles
Senior Contributor I

Hi,

I am looking at the interrupt table in the i.MX6Q reference manual and the security manual (under NDA), and I don't see any entry about the interrupt of the TZASC component. I guess it might be one of the SNVS interrupt, but I don't know which one.

Can someone point me the correct interrupt number ?

Best,

V.

Labels (1)
Tags (4)
1 Solution
2,532 Views
vsiles
Senior Contributor I

Dear YuriMuhin_ng‌,

after failing to get the TZASC interrupt through the CSU interrupt, I plugged a debugger and saw that the triggered interrupt was in fact "140 ASC1 ASC1 interrupt request."

I just leave this here, for future readers.

Best regards,

V.

View solution in original post

4 Replies
2,532 Views
Yuri
NXP Employee
NXP Employee

Hello,

  CSU interrupt should be used.

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

------------------------------------------------------------------------------

0 Kudos
Reply
2,532 Views
vsiles
Senior Contributor I

Dear YuriMuhin_ng​,

the interruption table says:

CSU interrupt request 1. Indicates to the processor that one or more alarm inputs were

asserted.

However I find no other mention of a CSU interrupt. I guess it is a "OR" of several interrupts, one of them being the TZASC. Is there a list of all the sources that might raise the CSU interrupt ?

Best,

Vincent

0 Kudos
Reply
2,532 Views
Yuri
NXP Employee
NXP Employee

Hello,

   " ... the CSU manages system security alarms. These alarms are signals routed from
various SoC peripherals and I/O that indicate security violation conditions".

   Please refer to the "Security Reference Manual for i.MX6Dual, 6Quad, 6Solo, and 6DualLite"

for more details what SoC peripherals and I/O are affected.

Regards,

Yuri.

0 Kudos
Reply
2,533 Views
vsiles
Senior Contributor I

Dear YuriMuhin_ng‌,

after failing to get the TZASC interrupt through the CSU interrupt, I plugged a debugger and saw that the triggered interrupt was in fact "140 ASC1 ASC1 interrupt request."

I just leave this here, for future readers.

Best regards,

V.