imx6q android 4.4.2 boot error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q android 4.4.2 boot error

2,995 Views
clound920419
Contributor I

Hi,

I recently downloaded Android 4.4.2 source code and  applied patch file successfully provided by freescale. After that, I compiled source code  and put the kernel image into the tftp server root directory and the generated Android file system files into the nfs server root directory. Board is booting but I am getting zygote issue so that I am not able to see a android boot logo and home screen, only four small penguin icon appears on the screen, serial port can be entered.  Kindly find attached log files for more information. Kindly help me to resolve the problem.

Thanks.

D/AndroidRuntime( 7765): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<

D/AndroidRuntime( 7765): CheckJNI is ON

I/AndroidRuntime( 7765): JNI options: '-Xjniopts:warnonly'

W/audio_hw_primary( 7766): in rate 44100, channels 1 format 0

I/AudioFlinger( 7766): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1

W/audio_hw_primary( 7766): open output stream devices 2, format 1, channels 3, sample_rate 44100, flag 2

W/audio_hw_primary( 7766): opened out stream...1074489432

I/AudioFlinger( 7766): HAL output buffer size 192 frames, normal mix buffer size 768 frames

I/AudioMixer( 7766): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

E/MonoPipe( 7766): Failed to fetch local time frequency when constructing a MonoPipe (res = -32).  getNextWriteTimestamp calls will be non-functional

I/ServiceManager( 2082): service 'media.audio_flinger' died

I/ServiceManager( 2082): service 'media.player' died

I/ServiceManager( 2082): service 'media.camera' died

I/Netd    ( 7857): Netd 1.0 starting

W/InterfaceController( 7857): Warning (dlopen failed: library "/system/lib/libnetcmdiface.so" not found) while opening the net interface command library

I/SurfaceFlinger( 7858): SurfaceFlinger is starting

I/SurfaceFlinger( 7858): SurfaceFlinger's main thread ready to run. Initializing graphics H/W...

D/libEGL  ( 7858): loaded /system/lib/egl/libEGL_VIVANTE.so

F/libc    ( 7858): Fatal signal 11 (SIGSEGV) at 0x000000d4 (code=1), thread 7858 (surfaceflinger)

I/mediaserver( 7860): ServiceManager: 0x40c93470

I/AudioFlinger( 7860): Using default 3000 mSec as standby time.

I/CameraService( 7860): CameraService started (pid=7860)

I/CameraService( 7860): Loaded "Freescale CameraHal Module" camera module

I/FslCameraHAL( 7860): Face Back Camera is ov5640_mipi, orient is 0

I/FslCameraHAL( 7860): Face Front Camera is uvc,ov5642_camera,ov5640_camera, orient is 0

I/FslCameraHAL( 7860): Checking the camera ov5640_mipi

I/FslCameraHAL( 7860): Checking the camera uvc

I/FslCameraHAL( 7860): Checking the camera ov5642_camera

I/FslCameraHAL( 7860): Checking the camera ov5640_camera

I/AudioPolicyManagerBase( 7860): loadAudioPolicyConfig() loaded /system/etc/audio_policy.conf

W/audio_hw_primary( 7860): card 0, id wm8974audio ,driver wm8974-audio, name wm8974-audio

W/audio_hw_primary( 7860): out rate 44100

D/AndroidRuntime( 7859):

D/AndroidRuntime( 7859): >>>>>> AndroidRuntime START com.android.internal.os.ZygoteInit <<<<<<

D/AndroidRuntime( 7859): CheckJNI is ON

I/AndroidRuntime( 7859): JNI options: '-Xjniopts:warnonly'

W/audio_hw_primary( 7860): in rate 44100, channels 1 format 0

I/AudioFlinger( 7860): loadHwModule() Loaded primary audio interface from Freescale i.MX Audio HW HAL (audio) handle 1

W/audio_hw_primary( 7860): open output stream devices 2, format 1, channels 3, sample_rate 44100, flag 2

W/audio_hw_primary( 7860): opened out stream...1074644864

I/AudioFlinger( 7860): HAL output buffer size 192 frames, normal mix buffer size 768 frames

I/AudioMixer( 7860): found effect "Multichannel Downmix To Stereo" from The Android Open Source Project

E/MonoPipe( 7860): Failed to fetch local time frequency when constructing a MonoPipe (res = -32).  getNextWriteTimestamp calls will be non-functional

I/DEBUG   ( 2085): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** ***

I/DEBUG   ( 2085): Build fingerprint: 'Freescale/sabresd_6dq/sabresd_6dq:4.4.2/1.0.0-rc3/20140630:eng/dev-keys'

I/DEBUG   ( 2085): Revision: '405525'

I/DEBUG   ( 2085): pid: 7858, tid: 7858, name: surfaceflinger  >>> /system/bin/surfaceflinger <<<

I/DEBUG   ( 2085): signal 11 (SIGSEGV), code 1 (SEGV_MAPERR), fault addr 000000d4

I/DEBUG   ( 2085):     r0 00000000  r1 40fed4e4  r2 ffffffd8  r3 404cdee8

I/DEBUG   ( 2085):     r4 00000000  r5 40fed4a8  r6 000030a0  r7 4021eb89

I/DEBUG   ( 2085):     r8 000000ac  r9 40238750  sl 00000001  fp 40238764

I/DEBUG   ( 2085):     ip 400b8edc  sp bea0f828  lr 400ae395  pc 4046203e  cpsr 00070030

I/DEBUG   ( 2085):     d0  0000000000000000  d1  0000000000000000

I/DEBUG   ( 2085):     d2  0000000000000000  d3  0000000000000000

I/DEBUG   ( 2085):     d4  0000000000000000  d5  0000000000000000

I/DEBUG   ( 2085):     d6  0000000000000000  d7  0000000000000000

I/DEBUG   ( 2085):     d8  0000000000000000  d9  0000000000000000

I/DEBUG   ( 2085):     d10 0000000000000000  d11 0000000000000000

I/DEBUG   ( 2085):     d12 0000000000000000  d13 0000000000000000

I/DEBUG   ( 2085):     d14 0000000000000000  d15 0000000000000000

I/DEBUG   ( 2085):     d16 41be2a7a5f97ced9  d17 3f50624dd2f1a9fc

I/DEBUG   ( 2085):     d18 4197eb05a4000000  d19 0000000000000000

I/DEBUG   ( 2085):     d20 0000000000000000  d21 0000000000000000

I/DEBUG   ( 2085):     d22 0000000000000000  d23 0000000000000000

I/DEBUG   ( 2085):     d24 0000000000000000  d25 0000000000000000

I/DEBUG   ( 2085):     d26 0000000000000000  d27 0000000000000000

I/DEBUG   ( 2085):     d28 0000000000000000  d29 0000000000000000

I/DEBUG   ( 2085):     d30 0000000000000000  d31 0000000000000000

I/DEBUG   ( 2085):     scr 00000010

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): backtrace:

I/DEBUG   ( 2085):     #00  pc 0002d03e  /system/lib/libGAL.so (gcoHAL_QueryChipCount+9)

I/DEBUG   ( 2085):     #01  pc 00002391  /system/lib/egl/libEGL_VIVANTE.so

I/DEBUG   ( 2085):     #02  pc 00006221  /system/lib/egl/libEGL_VIVANTE.so (eglGetProcAddress+12)

I/DEBUG   ( 2085):     #03  pc 00034921  /system/lib/libEGL.so

I/DEBUG   ( 2085):     #04  pc 000349f3  /system/lib/libEGL.so

I/DEBUG   ( 2085):     #05  pc 0000dc49  /system/lib/libEGL.so

I/DEBUG   ( 2085):     #06  pc 0000e351  /system/lib/libEGL.so (eglGetDisplay+24)

I/DEBUG   ( 2085):     #07  pc 0001b537  /system/lib/libsurfaceflinger.so (android::SurfaceFlinger::init()+46)

I/DEBUG   ( 2085):     #08  pc 000008a7  /system/bin/surfaceflinger

I/DEBUG   ( 2085):     #09  pc 0000e423  /system/lib/libc.so (__libc_init+50)

I/DEBUG   ( 2085):     #10  pc 000007dc  /system/bin/surfaceflinger

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): stack:

I/DEBUG   ( 2085):          bea0f7e8  40129ea5  /system/lib/libc.so (dlmalloc)

I/DEBUG   ( 2085):          bea0f7ec  bea0f830  [stack]

I/DEBUG   ( 2085):          bea0f7f0  000000a8 

I/DEBUG   ( 2085):          bea0f7f4  40fecc18  [heap]

I/DEBUG   ( 2085):          bea0f7f8  4021eb89  /system/lib/libEGL.so

I/DEBUG   ( 2085):          bea0f7fc  000000ac 

I/DEBUG   ( 2085):          bea0f800  40238750 

I/DEBUG   ( 2085):          bea0f804  00000001 

I/DEBUG   ( 2085):          bea0f808  40238764 

I/DEBUG   ( 2085):          bea0f80c  40127cd1  /system/lib/libc.so (malloc+12)

I/DEBUG   ( 2085):          bea0f810  40fed4a8  [heap]

I/DEBUG   ( 2085):          bea0f814  00000000 

I/DEBUG   ( 2085):          bea0f818  4021eb89  /system/lib/libEGL.so

I/DEBUG   ( 2085):          bea0f81c  40fecc18  [heap]

I/DEBUG   ( 2085):          bea0f820  4021eb89  /system/lib/libEGL.so

I/DEBUG   ( 2085):          bea0f824  400ae36b  /system/lib/egl/libEGL_VIVANTE.so

I/DEBUG   ( 2085):     #00  bea0f828  40fed470  [heap]

I/DEBUG   ( 2085):          ........  ........

I/DEBUG   ( 2085):     #01  bea0f828  40fed470  [heap]

I/DEBUG   ( 2085):          bea0f82c  401134b9  /system/bin/linker

I/DEBUG   ( 2085):          bea0f830  40fed4a8  [heap]

I/DEBUG   ( 2085):          bea0f834  00000001 

I/DEBUG   ( 2085):          bea0f838  bea0f9ec  [stack]

I/DEBUG   ( 2085):          bea0f83c  40109979  /system/bin/linker

I/DEBUG   ( 2085):          bea0f840  400a26dc 

I/DEBUG   ( 2085):          bea0f844  400796dc 

I/DEBUG   ( 2085):          bea0f848  400b8e7c  /system/lib/egl/libEGL_VIVANTE.so

I/DEBUG   ( 2085):          bea0f84c  400ad444  /system/lib/egl/libEGL_VIVANTE.so

I/DEBUG   ( 2085):          bea0f850  00000068 

I/DEBUG   ( 2085):          bea0f854  04f9f9f2 

I/DEBUG   ( 2085):          bea0f858  00000083 

I/DEBUG   ( 2085):          bea0f85c  40108003  /system/bin/linker

I/DEBUG   ( 2085):          bea0f860  400796dc 

I/DEBUG   ( 2085):          bea0f864  4021eb89  /system/lib/libEGL.so

I/DEBUG   ( 2085):          ........  ........

I/DEBUG   ( 2085):     #02  bea0f880  00000000 

I/DEBUG   ( 2085):          bea0f884  400796dc 

I/DEBUG   ( 2085):          bea0f888  ffffffff 

I/DEBUG   ( 2085):          bea0f88c  40107f13  /system/bin/linker

I/DEBUG   ( 2085):          bea0f890  400796dc 

I/DEBUG   ( 2085):          bea0f894  400796dc 

I/DEBUG   ( 2085):          bea0f898  4021eb89  /system/lib/libEGL.so

I/DEBUG   ( 2085):          bea0f89c  40fecc18  [heap]

I/DEBUG   ( 2085):          bea0f8a0  40230de8  /system/lib/libEGL.so

I/DEBUG   ( 2085):          bea0f8a4  40218923  /system/lib/libEGL.so

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): memory near r1:

I/DEBUG   ( 2085):     40fed4c4 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed4d4 00000000 00000000 00000000 00000001 

I/DEBUG   ( 2085):     40fed4e4 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed4f4 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed504 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed514 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed524 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed534 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed544 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed554 00000751 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed564 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed574 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed584 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed594 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed5a4 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed5b4 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): memory near r3:

I/DEBUG   ( 2085):     404cdec8 ffffffff 00000000 3f800000 00000000 

I/DEBUG   ( 2085):     404cded8 00000000 00000000 3f800000 00000000 

I/DEBUG   ( 2085):     404cdee8 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     404cdef8 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     404cdf08 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     404cdf18 00000000 000000d4 00000000 00000000 

I/DEBUG   ( 2085):     404cdf28 00000000 00000000 00000000 00000002 

I/DEBUG   ( 2085):     404cdf38 00000007 00030201 00000000 40490bf5 

I/DEBUG   ( 2085):     404cdf48 00000001 00000002 00000104 00000000 

I/DEBUG   ( 2085):     404cdf58 00000000 ffffffff 00000001 03000204 

I/DEBUG   ( 2085):     404cdf68 00000000 40490cc1 00000002 0000000a 

I/DEBUG   ( 2085):     404cdf78 00030201 00000000 40490bf5 00000001 

I/DEBUG   ( 2085):     404cdf88 00000002 00000104 00000000 00000000 

I/DEBUG   ( 2085):     404cdf98 ffffffff 00000001 fd000204 00000000 

I/DEBUG   ( 2085):     404cdfa8 40490cc1 00000002 00000008 00030201 

I/DEBUG   ( 2085):     404cdfb8 00000000 40490bf5 00000001 00000002 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): memory near r5:

I/DEBUG   ( 2085):     40fed488 400ae2ad 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed498 00000000 00000000 00000000 000000b3 

I/DEBUG   ( 2085):     40fed4a8 00000000 00003000 000030a0 00000000 

I/DEBUG   ( 2085):     40fed4b8 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed4c8 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed4d8 00000000 00000000 00000001 00000000 

I/DEBUG   ( 2085):     40fed4e8 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed4f8 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed508 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed518 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed528 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed538 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed548 00000000 00000000 00000000 00000751 

I/DEBUG   ( 2085):     40fed558 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed568 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40fed578 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): memory near r6:

I/DEBUG   ( 2085):     00003080 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     00003090 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     000030a0 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     000030b0 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     000030c0 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     000030d0 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     000030e0 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     000030f0 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     00003100 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     00003110 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     00003120 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     00003130 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     00003140 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     00003150 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     00003160 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):     00003170 ffffffff ffffffff ffffffff ffffffff 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): memory near r7:

I/DEBUG   ( 2085):     4021eb68 616e6769 6e79536c 52484b63 6c676500 

I/DEBUG   ( 2085):     4021eb78 53746547 41636e79 69727474 52484b62 

I/DEBUG   ( 2085):     4021eb88 6c676500 74696157 636e7953 0052484b 

I/DEBUG   ( 2085):     4021eb98 536c6765 77537465 65527061 6e617463 

I/DEBUG   ( 2085):     4021eba8 41656c67 4f52444e 65004449 65476c67 

I/DEBUG   ( 2085):     4021ebb8 6e655274 42726564 65666675 444e4172 

I/DEBUG   ( 2085):     4021ebc8 44494f52 6c676500 4e707544 76697461 

I/DEBUG   ( 2085):     4021ebd8 6e654665 44466563 52444e41 0044494f 

I/DEBUG   ( 2085):     4021ebe8 476c6765 79537465 6d657473 656d6954 

I/DEBUG   ( 2085):     4021ebf8 71657246 636e6575 00564e79 476c6765 

I/DEBUG   ( 2085):     4021ec08 79537465 6d657473 656d6954 6500564e 

I/DEBUG   ( 2085):     4021ec18 69486c67 6e726562 50657461 65636f72 

I/DEBUG   ( 2085):     4021ec28 4d497373 67650047 6177416c 506e656b 

I/DEBUG   ( 2085):     4021ec38 65636f72 4d497373 6c670047 69746341 

I/DEBUG   ( 2085):     4021ec48 68536576 72656461 676f7250 456d6172 

I/DEBUG   ( 2085):     4021ec58 67005458 7463416c 54657669 75747865 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): memory near r9:

I/DEBUG   ( 2085):     40238730 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40238740 00000000 00000000 00000000 00000001 

I/DEBUG   ( 2085):     40238750 00000000 40236e64 40237ad8 00000000 

I/DEBUG   ( 2085):     40238760 00000000 400b0ed9 400b1d2d 400b1dad 

I/DEBUG   ( 2085):     40238770 400aee3d 400aef85 400aef89 400b3591 

I/DEBUG   ( 2085):     40238780 400b4385 400b3929 400b3809 400b4025 

I/DEBUG   ( 2085):     40238790 400afd25 400aff71 400aff6d 400b210d 

I/DEBUG   ( 2085):     402387a0 400b20d1 400b20c1 400b1fbd 400b00b9 

I/DEBUG   ( 2085):     402387b0 400b218d 400b4fe5 400b5431 400b0ec5 

I/DEBUG   ( 2085):     402387c0 400b1e79 400b2215 400b3ecd 400b4569 

I/DEBUG   ( 2085):     402387d0 400b4645 400b2145 400afcb9 400afd11 

I/DEBUG   ( 2085):     402387e0 400b0145 400b008d 400b3c89 400b46f9 

I/DEBUG   ( 2085):     402387f0 400b47c1 400b0a89 400b0c51 400b572d 

I/DEBUG   ( 2085):     40238800 400b584d 400b58cd 400b5991 400b5a2d 

I/DEBUG   ( 2085):     40238810 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40238820 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): memory near fp:

I/DEBUG   ( 2085):     40238744 00000000 00000000 00000001 00000000 

I/DEBUG   ( 2085):     40238754 40236e64 40237ad8 00000000 00000000 

I/DEBUG   ( 2085):     40238764 400b0ed9 400b1d2d 400b1dad 400aee3d 

I/DEBUG   ( 2085):     40238774 400aef85 400aef89 400b3591 400b4385 

I/DEBUG   ( 2085):     40238784 400b3929 400b3809 400b4025 400afd25 

I/DEBUG   ( 2085):     40238794 400aff71 400aff6d 400b210d 400b20d1 

I/DEBUG   ( 2085):     402387a4 400b20c1 400b1fbd 400b00b9 400b218d 

I/DEBUG   ( 2085):     402387b4 400b4fe5 400b5431 400b0ec5 400b1e79 

I/DEBUG   ( 2085):     402387c4 400b2215 400b3ecd 400b4569 400b4645 

I/DEBUG   ( 2085):     402387d4 400b2145 400afcb9 400afd11 400b0145 

I/DEBUG   ( 2085):     402387e4 400b008d 400b3c89 400b46f9 400b47c1 

I/DEBUG   ( 2085):     402387f4 400b0a89 400b0c51 400b572d 400b584d 

I/DEBUG   ( 2085):     40238804 400b58cd 400b5991 400b5a2d 00000000 

I/DEBUG   ( 2085):     40238814 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40238824 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):     40238834 00000000 00000000 00000000 00000000 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): memory near ip:

I/DEBUG   ( 2085):     400b8ebc 40142e99 40142da5 4046d299 4046eab9 

I/DEBUG   ( 2085):     400b8ecc 4046d4c1 4046de15 4046d48d 4013c5b8 

I/DEBUG   ( 2085):     400b8edc 40462035 4046207d 40462159 4045b5a9 

I/DEBUG   ( 2085):     400b8eec 4046d2d9 40461f11 4046dcbd 4046dd91 

I/DEBUG   ( 2085):     400b8efc 40466ff5 4046671d 4045b1c9 4013c0c4 

I/DEBUG   ( 2085):     400b8f0c 40468aad 40468b19 40468cf9 404682b5 

I/DEBUG   ( 2085):     400b8f1c 40466411 4046891d 4046f3dd 4045c1ad 

I/DEBUG   ( 2085):     400b8f2c 40468e61 40468965 40461ff5 4046ea0d 

I/DEBUG   ( 2085):     400b8f3c 4045b65d 40468e71 40468925 40466305 

I/DEBUG   ( 2085):     400b8f4c 401549c0 40468e41 404664f1 404666e1 

I/DEBUG   ( 2085):     400b8f5c 404667b9 404668d5 4046f49d 4046eab5 

I/DEBUG   ( 2085):     400b8f6c 4046ea2d 4046f321 4046d9b1 4046f3a1 

I/DEBUG   ( 2085):     400b8f7c 4046d979 4046ea51 4046ddad 4046d9a1 

I/DEBUG   ( 2085):     400b8f8c 4046f365 4046d9f9 4046d4c1 4046da7d 

I/DEBUG   ( 2085):     400b8f9c 40466685 40461d89 4045b129 40468935 

I/DEBUG   ( 2085):     400b8fac 40468719 404666fd 4045b09d 4045c2c1 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): memory near sp:

I/DEBUG   ( 2085):     bea0f808 40238764 40127cd1 40fed4a8 00000000 

I/DEBUG   ( 2085):     bea0f818 4021eb89 40fecc18 4021eb89 400ae36b 

I/DEBUG   ( 2085):     bea0f828 40fed470 401134b9 40fed4a8 00000001 

I/DEBUG   ( 2085):     bea0f838 bea0f9ec 40109979 400a26dc 400796dc 

I/DEBUG   ( 2085):     bea0f848 400b8e7c 400ad444 00000068 04f9f9f2 

I/DEBUG   ( 2085):     bea0f858 00000083 40108003 400796dc 4021eb89 

I/DEBUG   ( 2085):     bea0f868 40fecc18 4021eb89 000000ac 40238750 

I/DEBUG   ( 2085):     bea0f878 00000001 400b2225 00000000 400796dc 

I/DEBUG   ( 2085):     bea0f888 ffffffff 40107f13 400796dc 400796dc 

I/DEBUG   ( 2085):     bea0f898 4021eb89 40fecc18 40230de8 40218923 

I/DEBUG   ( 2085):     bea0f8a8 00000004 00000000 00000013 4022fc88 

I/DEBUG   ( 2085):     bea0f8b8 40fedcb8 40fec900 00000004 40238750 

I/DEBUG   ( 2085):     bea0f8c8 40fecc18 40fecc18 00000000 400a484d 

I/DEBUG   ( 2085):     bea0f8d8 40feb52c 00000000 bea0f9ec 402189f7 

I/DEBUG   ( 2085):     bea0f8e8 00000000 40238750 40fecc18 402394ec 

I/DEBUG   ( 2085):     bea0f8f8 40163fd8 401f1c4d 00000000 bea0f968 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): code around pc:

I/DEBUG   ( 2085):     4046201c db042800 9b00b12c 68192000 b0026021 

I/DEBUG   ( 2085):     4046202c 4620bd10 bf00e7fb 4a084b07 589b447b 

I/DEBUG   ( 2085):     4046203c f8d06858 1e5a30d4 d8022a02 2000600b 

I/DEBUG   ( 2085):     4046204c f06f4770 47700008 0006ae28 ffffffd8 

I/DEBUG   ( 2085):     4046205c 4a064b05 589b447b f8d06858 1c0810e4 

I/DEBUG   ( 2085):     4046206c 2001bf18 bf004770 0006ae00 ffffffd8 

I/DEBUG   ( 2085):     4046207c 2300b570 4833b08e 46152902 93044478 

I/DEBUG   ( 2085):     4046208c bfc89306 9308461c dc05930a 31364a2e 

I/DEBUG   ( 2085):     4046209c 68445880 4021f854 f00ba80c 2800feb5 

I/DEBUG   ( 2085):     404620ac bfa4a80c 680e990c feaef00b bfa42800 

I/DEBUG   ( 2085):     404620bc 601c9b0c f04fb91c b00e30ff 2c03bd70 

I/DEBUG   ( 2085):     404620cc 2400d815 9400a804 94014621 94024622 

I/DEBUG   ( 2085):     404620dc 94034623 fa7af7f2 dbee2800 a908a806 

I/DEBUG   ( 2085):     404620ec ab0a4622 fb22f7f2 da172800 2c04e7e5 

I/DEBUG   ( 2085):     404620fc 2400d1e1 9400a904 94014620 46234622 

I/DEBUG   ( 2085):     4046210c fa4cf058 dbd82800 4620aa0a a9069200 

I/DEBUG   ( 2085):

I/DEBUG   ( 2085): code around lr:

I/DEBUG   ( 2085):     400ae374 013cf105 447e615d f44f619e 63aa5640 

I/DEBUG   ( 2085):     400ae384 36a0606e 40a0f8c5 601a60ae eda8f7ff 

I/DEBUG   ( 2085):     400ae394 dbc32800 28006be8 e0cedc03 42a36beb 

I/DEBUG   ( 2085):     400ae3a4 1ca3dd0a 20004621 eb053401 f7ff1243 

I/DEBUG   ( 2085):     400ae3b4 2800ed9e e7b1daf2 f3402b00 f10380be 

I/DEBUG   ( 2085):     400ae3c4 f8d534ff 69afe014 0c94ea4f f1bc69ee 

I/DEBUG   ( 2085):     400ae3d4 bf180f00 ea4f2b03 bf8c088c 20012000 

I/DEBUG   ( 2085):     400ae3e4 80aef240 eb10eea6 0250f105 7b10eea4 

I/DEBUG   ( 2085):     400ae3f4 6b10eea2 f1024611 f9610a20 f1020a8d 

I/DEBUG   ( 2085):     400ae404 f1020930 f1020e40 f1020750 f1020660 

I/DEBUG   ( 2085):     400ae414 f9610470 30018a8f 45843280 ea8ff96a 

I/DEBUG   ( 2085):     400ae424 2a8ff969 6a8ff96e aa8ff967 ca8ff966 

I/DEBUG   ( 2085):     400ae434 4a8ff964 0168fffa e162fffa 616afffa 

I/DEBUG   ( 2085):     400ae444 c164fffa 8162fffa a164fffa 016efffa 

I/DEBUG   ( 2085):     400ae454 616cfffa 816afffa 0166fffa 4668ef24 

I/DEBUG   ( 2085):     400ae464 2164fffa 6660ef26 2662ef22 ef22d8c2

0 Kudos
Reply
2 Replies

2,183 Views
igorpadykov
NXP Employee
NXP Employee

Hi clound920419

suggest to try to boot Demo Images:

Board Support Packages (35)

IMX6_SABRE_SD_KK442_100_ANDROID_DEMO_BSP (REV KK4.4.2_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Also please recheck attached document sect.4.2 System on NFS, sect.3.5 Building kernel image

and try Demo Images using Table 4. Images for SABRE-SD TFTP and NFS.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,183 Views
clound920419
Contributor I

Hi igorpadykov,

As you say, I have rechecked the attached document sect.4.2 System on NFS, sect.3.5 Building kernel image

and try Demo Android file system for my own board using TFTP and NFS. For the kernel source,  I just changed arch/arm/mach-mx6/board-mx6q_sabrelite.c and added some kernel drivers, the ERROR always exits.

For the logcat BT information:

I/DEBUG   ( 2087):     #00  pc 0002d394  /system/lib/libGAL.so (gcoHAL_QueryChipCount+7)

I/DEBUG   ( 2087):     #01  pc 00002303  /system/lib/egl/libEGL_VIVANTE.so

I/DEBUG   ( 2087):     #02  pc 00006131  /system/lib/egl/libEGL_VIVANTE.so (eglGetProcAddress+12)

I/DEBUG   ( 2087):     #03  pc 00034921  /system/lib/libEGL.so

I/DEBUG   ( 2087):     #04  pc 000349f3  /system/lib/libEGL.so

I/DEBUG   ( 2087):     #05  pc 0000dc49  /system/lib/libEGL.so

I/DEBUG   ( 2087):     #06  pc 0000e351  /system/lib/libEGL.so (eglGetDisplay+24)

I/DEBUG   ( 2087):     #07  pc 0001b537  /system/lib/libsurfaceflinger.so (android::SurfaceFlinger::init()+46)

I/DEBUG   ( 2087):     #08  pc 000008a7  /system/bin/surfaceflinger

I/DEBUG   ( 2087):     #09  pc 0000e423  /system/lib/libc.so (__libc_init+50)

I/DEBUG   ( 2087):     #10  pc 000007dc  /system/bin/surfaceflinger

It's call eglGetDisplay() function to get OpenGL lib's default screen failed, any reason about it?

thanks

clound

0 Kudos
Reply