imx6q MII RGMII

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q MII RGMII

2,794 次查看
eliaz
Contributor II

Can the imx6q use RGMII & MII peripheries  in the same time (Can these peripheries be active in the same time)?

标签 (2)
0 项奖励
回复
4 回复数

2,575 次查看
eliaz
Contributor II

can you be more specific about multiplexing , which signal is shared between the interfaces?

0 项奖励
回复

2,575 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

 IMX6Q has ENET module, which supports MII, RMII, RGMII interfaces

Pins affected are described in Table 23-1 (ENET External Signals) of

the i.MX6 RM (Rev. 3, 07/2015). Only single interface may be used

at a time because of multiplexing. 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 项奖励
回复

2,575 次查看
eliaz
Contributor II

can you be more specific about multiplexing , which signal is shared between the interfaces?

0 项奖励
回复

2,575 次查看
eliaz
Contributor II

can you be more specific about multiplexing , which signal is shared between the interfaces?

0 项奖励
回复