imx6q) How to test SPI, UART, CAN ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q) How to test SPI, UART, CAN ?

4,870 Views
ktc7270
Contributor II

HI,

I want to test imx6q-sabresd. The device driver seems to be properly configured.

I want to know if there are test codes.

For example, the test code can transfer the spi data of the imx6 board to another board.

(The data received from the imx6 board can do something else through the test code.

Please help me.

ps. add questions.

Labels (2)
2 Replies

4,275 Views
winy2014
Contributor II

Hi,

if users use i.MX6Q board designed by Forlinx, generally the related codes are provided.

Rgds,

Grace

0 Kudos
Reply

4,272 Views
igorpadykov
NXP Employee
NXP Employee

Hi kangta

for testing one can use unit tests described in Chapter 9 Unit Tests attached Linux Manual

imx-test
https://source.codeaurora.org/external/imx/imx-test/tree/?h=imx_4.9.88_2.0.0_ga

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------