imx6dl - gstreamer h264parse

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6dl - gstreamer h264parse

4,164 Views
jefflancaster
Contributor I

I installed gstreamer-0.10 on my qt4 project.

I installed gst-plugins-bad_0.10.23-r4_cortexa9hf-vfp-neon.ipk and it posted the following text:

Installed gst-plugins-bad:

~# opkg install gst-plugins-bad_0.10.23-r4_cortexa9hf-vfp-neon.ipk

Installing gst-plugins-bad (0.10.23-r4) to root...

Configuring gst-plugins-bad.

warning: Schema 'org.freedesktop.gstreamer-0.10.default-elements' has path '/desktop/gstreamer/0.10/default-elements/'.  Paths starting with '/apps/', '/desktop/' or '/system/' are deprecated.

The warning didn't concern me too much until I installed gst-plugins-bad-h264parse_0.10.23-r4_cortexa9hf-vfp-neon.ipk and tried to use it.

Installed h264parse:

~# opkg install gst-plugins-bad-h264parse_0.10.23-r4_cortexa9hf-vfp-neon.ipk

Installing gst-plugins-bad-h264parse (0.10.23-r4) to root...

Configuring gst-plugins-bad-h264parse.

Ran pipeline:

gst-launch -v gstrtpbin name=rtpbin rtspsrc location=rtsp://user:password@localhost:8554/Video-81 latency=500 ! rtph264depay ! h264parse ! fakesink name=sink

WARNING: erroneous pipeline: no element "h264parse"

For some reason I can't get h264parse to work and I think the warning given while installing gst-plugins-bad_... might be a hint.

The above pipeline runs just fine without h264parse.

Any thoughts?

Labels (2)
0 Kudos
Reply
1 Reply

1,838 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jeff

one can look at sect.7.3 Multimedia use cases attached Linux Guide

what is supported for gst-launch in L3.14.28_1.0.0_iMX6QDLS_BUNDLE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply