imx6dl:android4.4.2:Repeat reboot kernel panic

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6dl:android4.4.2:Repeat reboot kernel panic

1,479 次查看
zmnqaz
Contributor I

Executive command "reboot" about 50~60, kernel will panic.

I don't know why  can not find /dev/xxxx

init: watchdogd: Failed to open /dev/watchdog: No such file or directory

 

U-Boot 2009.08-dirty (Sep 22 2016 - 11:20:41)

CPU: Freescale i.MX6 family TO1.3 at 792 MHz
Thermal sensor with ratio = 185
Temperature: 71 C, calibration data 0x59550469
mx6q pll1: 792MHz
mx6q pll2: 528MHz
mx6q pll3: 480MHz
mx6q pll8: 50MHz
ipg clock : 66000000Hz
ipg per clock : 66000000Hz
uart clock : 80000000Hz
cspi clock : 60000000Hz
ahb clock : 132000000Hz
axi clock : 198000000Hz
emi_slow clock: 99000000Hz
ddr clock : 396000000Hz
usdhc1 clock : 198000000Hz
usdhc2 clock : 198000000Hz
usdhc3 clock : 198000000Hz
usdhc4 clock : 198000000Hz
nfc clock : 24000000Hz
Board: i.MX6DL/Solo-SABRESD: unknown-board Board: 0x61013 [WDOG ]
Boot Device: MMC
I2C: ready
DRAM: 1 GB
MMC: FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3
In: serial
Out: serial
Err: serial
Found PFUZE100! deviceid=10,revid=21
update key pressed check........
Net: got MAC address from IIM: 00:95:69:77:0d:f5
FEC0 [PRIME]
Hit any key to stop autoboot: 0
kernel @ 10808000 (4792476)
ramdisk @ 11800000 (499984)
kernel cmdline:
use uboot command line:
console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,1280x800@60,if=RGB24,bpp=32 ldb=sin0 video=mxcfb1:off video=mxcfb2:off fbmem=32M vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale ldo_active=on

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
Initializing cgroup subsys cpu
Linux version 3.0.35-gccd8e37 (u@u-VirtualBox) (gcc version 4.7 (GCC) ) #69 SMP PREEMPT Tue May 2 09:54:57 CST 2017
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board
Ignoring unrecognised tag 0x54410008
Memory policy: ECC disabled, Data cache writealloc
CPU identified as i.MX6DL/SOLO, unknown revision
PERCPU: Embedded 7 pages/cpu @c12e4000 s6528 r8192 d13952 u32768
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 202496
Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,1280x800@60,if=RGB24,bpp=32 ldb=sin0 video=mxcfb1:off video=mxcfb2:off fbmem=32M vmalloc=400M androidboot.console=ttymxc0 androidboot.hardware=freescale ldo_active=on
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 767MB 32MB = 799MB total
Memory: 797880k/797880k available, 250696k reserved, 408576K highmem
Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
DMA : 0xfbe00000 - 0xffe00000 ( 64 MB)
vmalloc : 0xd9800000 - 0xf2000000 ( 392 MB)
lowmem : 0xc0000000 - 0xd9000000 ( 400 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.init : 0xc0008000 - 0xc0046000 ( 248 kB)
.text : 0xc0046000 - 0xc08bc024 (8665 kB)
.data : 0xc08be000 - 0xc094de88 ( 576 kB)
.bss : 0xc094deac - 0xc0ada8f0 (1587 kB)
Preemptible hierarchical RCU implementation.
NR_IRQS:624
MXC GPIO hardware
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms
Set periph_clk's parent to pll2_pfd_400M!
arm_max_freq=1GHz
MXC_Early serial console at MMIO 0x2020000 (options '115200')
bootconsole [ttymxc0] enabled
Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux: Initializing.
Mount-cache hash table entries: 512
Initializing cgroup subsys debug
Initializing cgroup subsys cpuacct
Initializing cgroup subsys freezer
CPU: Testing write buffer coherency: ok
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
CPU1: Booted secondary processor
Brought up 2 CPUs
SMP: Total of 2 processors activated (3162.11 BogoMIPS).
print_constraints: dummy:
NET: Registered protocol family 16
print_constraints: vddpu: 725 <--> 1300 mV at 700 mV fast normal
print_constraints: vddcore: 725 <--> 1300 mV at 1150 mV fast normal
print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal
print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal
print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal
print_constraints: vdd3p0: 2625 <--> 3400 mV at 3000 mV fast normal
ram_console: got buffer at 3ff00000, size 100000
ram_console: found existing buffer, size 24407, start 24407
console [ram-1] enabled
hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.
hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.
hw-breakpoint: maximum watchpoint size is 4 bytes.
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32050000, Cache size: 524288 B
bio: create slab <bio-0> at 0
mxs-dma mxs-dma-apbh: initialized
print_constraints: VDDA: 3300 mV
print_constraints: VDDIO: 3300 mV
print_constraints: VDDD: 1200 mV
print_constraints: vmmc: 3300 mV
vgaarb: loaded
SCSI subsystem initialized
spi_imx imx6q-ecspi.0: probed
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Freescale USB OTG Driver loaded, $Revision: 1.55 $
mc_pfuze 1-0008: ID: 0,Full lay: 2 ,Metal lay: 1
mc_pfuze 1-0008: FAB: 0 ,FIN: 0
print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1375 mV
print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV
print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1375 mV
print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV
print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV
print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV
print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV
print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV
print_constraints: PFUZE100_VREFDDR: at 750 mV
print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV
print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2800 mV
print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV
print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 3000 mV
print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV
imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Version 1.0.24.
cfg80211: Calling CRDA to update world regulatory domain
Switching to clocksource mxc_timer1
NET: Registered protocol family 2
IP route cache hash table entries: 16384 (order: 4, 65536 bytes)
TCP established hash table entries: 65536 (order: 7, 524288 bytes)
TCP bind hash table entries: 65536 (order: 7, 786432 bytes)
TCP: Hash tables configured (established 65536 bind 65536)
TCP reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
PCI: CLS 0 bytes, default 32
Unpacking initramfs...
Freeing initrd memory: 488K
PMU: registered new PMU device of type 0
Static Power Management for Freescale i.MX6
wait mode is enabled for i.MX6
cpaddr = d9820000 suspend_iram_base=d98b4000
PM driver module loaded
IMX usb wakeup probe
the wakeup pdata is 0xd65f9b60
add wake up source irq 75
IMX usb wakeup probe
the wakeup pdata is 0xd65f9920
cpu regulator mode:ldo_enable
i.MXC CPU frequency driver
audit: initializing netlink socket (disabled)
type=2000 audit(0.940:1): initialized
highmem bounce pool size: 64 pages
ashmem: initialized
NTFS driver 2.1.30 [Flags: R/O].
JFFS2 version 2.2. (NAND) ?? 2001-2006 Red Hat, Inc.
fuse init (API version 7.16)
exFAT: Core Version 1.2.4
exFAT: FS Version 1.2.4
msgmni has been set to 761
SELinux: Registering netfilter hooks
NET: Registered protocol family 38
cryptodev: driver loaded.
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
#######request TFT gpio
mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed
MIPI DSI driver module loaded
mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb
_regulator_get: get() with no identifier
mxc_ldb mxc_ldb: change IPU DI1 to IPU DI0 for LDB channel0.
imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
mxc_sdc_fb mxc_sdc_fb.1: Can't get fb option for mxcfb1!
imx-sdma imx-sdma: loaded firmware 1.1
imx-sdma imx-sdma: initialized
Serial: IMX driver
imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX
imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
console [ttymxc0] enabled, bootconsole disabled
console [ttymxc0] enabled, bootconsole disabled
imx-uart.4: ttymxc4 at MMIO 0x21f4000 (irq = 62) is a IMX
imx-uart.3: ttymxc3 at MMIO 0x21f0000 (irq = 61) is a IMX
loop: module loaded
m25p80 spi0.0: unrecognized JEDEC id ffffff
GPMI NAND driver registered. (IMX)
vcan: Virtual CAN interface driver
CAN device driver interface
flexcan netdevice driver
FEC Ethernet Driver
fec_enet_mii_bus: probed
PPP generic driver version 2.4.2
PPP Deflate Compression module registered
PPP BSD Compression module registered
PPP MPPE Compression module registered
NET: Registered protocol family 24
tun: Universal TUN/TAP device driver, 1.6
tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
add wake up source irq 72
fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2
fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200
fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for FTDI USB Serial Device
usbcore: registered new interface driver ftdi_sio
ftdi_sio: v1.6.0:USB FTDI Serial Converters Driver
USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver option
option: v0.7.2:USB Driver for GSM modems
USB Serial support registered for Qualcomm USB modem
usbcore: registered new interface driver qcserial
ARC USBOTG Device Controller driver (1 August 2005)
android_usb gadget: Mass Storage Function, version: 2009/09/11
android_usb gadget: Number of LUNs=1
lun0: LUN: removable file: (no medium)
Gadget Android: controller 'fsl-usb2-udc' not recognized
android_usb gadget: android_usb ready
Suspend udc for OTG auto detect
USB Host suspend begins
will suspend roothub and its children
ehci_fsl_bus_suspend begins, DR
ehci_fsl_bus_suspend ends, DR
host suspend ends
USB Gadget resume begins
fsl_udc_resume, Wait for wakeup thread finishes
dr_controller_run: udc enter low power mode
USB Gadget resume ends
fsl-usb2-udc: bind to driver android_usb
mousedev: PS/2 mouse device common for all mice
input: gpio-keys as /devices/platform/gpio-keys/input/input0
cyttsp5_i2c_adapter 1-0024: cyttsp5_init: INIT CYTTSP RST gpio=111 and IRQ gpio=107 r=0
input: touch_key as /devices/virtual/input/input1
cyttsp5_i2c_adapter 1-0024: cyttsp5_probe: Error, device_init_wakeup rc:-17
cyttsp5_i2c_adapter 1-0024: cyttsp5_startup_: Bootloader mode
cyttsp5_i2c_adapter 1-0024: cyttsp5_hid_output_validate_bl_response: HID output response, ERROR:5
cyttsp5_i2c_adapter 1-0024: cyttsp5_startup_: Operational mode
cyttsp5_i2c_adapter 1-0024: cyttsp5_startup_: Reading report descriptor
usb 2-1: new high speed USB device number 2 using fsl-ehci
hub 2-1:1.0: USB hub found
hub 2-1:1.0: 4 ports detected
usb 2-1.2: new high speed USB device number 3 using fsl-ehci
USB Gadget resume begins
fsl_udc_resume, Wait for wakeup thread finishes
ftdi_sio 2-1.2:1.0: FTDI USB Serial Device converter detected
usb 2-1.2: Detected FT4232H
usb 2-1.2: Number of endpoints 2
usb 2-1.2: Endpoint 1 MaxPacketSize 512
usb 2-1.2: Endpoint 2 MaxPacketSize 512
usb 2-1.2: Setting MaxPacketSize 512
usb 2-1.2: FTDI USB Serial Device converter now attached to ttyUSB0
ftdi_sio 2-1.2:1.1: FTDI USB Serial Device converter detected
usb 2-1.2: Detected FT4232H
usb 2-1.2: Number of endpoints 2
usb 2-1.2: Endpoint 1 MaxPacketSize 512
usb 2-1.2: Endpoint 2 MaxPacketSize 512
usb 2-1.2: Setting MaxPacketSize 512
usb 2-1.2: FTDI USB Serial Device converter now attached to ttyUSB1
ftdi_sio 2-1.2:1.2: FTDI USB Serial Device converter detected
usb 2-1.2: Detected FT4232H
usb 2-1.2: Number of endpoints 2
usb 2-1.2: Endpoint 1 MaxPacketSize 512
usb 2-1.2: Endpoint 2 MaxPacketSize 512
usb 2-1.2: Setting MaxPacketSize 512
usb 2-1.2: FTDI USB Serial Device converter now attached to ttyUSB2
ftdi_sio 2-1.2:1.3: FTDI USB Serial Device converter detected
usb 2-1.2: Detected FT4232H
usb 2-1.2: Number of endpoints 2
usb 2-1.2: Endpoint 1 MaxPacketSize 512
usb 2-1.2: Endpoint 2 MaxPacketSize 512
usb 2-1.2: Setting MaxPacketSize 512
usb 2-1.2: FTDI USB Serial Device converter now attached to ttyUSB3
cyttsp5_i2c_adapter 1-0024: cyttsp5 Protocol Version: 1.2
input: cyttsp5_mt as /devices/platform/imx-i2c.1/i2c-1/1-0024/input/input2
cyttsp5_core_rt_suspend
cyttsp5_i2c_init: Cypress TTSP v5 I2C Driver (Built 20141006) rc=0
input: pwm-beeper as /devices/platform/pwm-beeper.0/input/input3
i2c-core: driver [isl29023] using legacy suspend method
i2c-core: driver [isl29023] using legacy resume method
hdc1000_init
msp430_adc_probe
rtc-pcf8563 2-0051: pcf8563_probe
rtc-pcf8563 2-0051: get_datetime.go
rtc-pcf8563 2-0051: pcf8563_get_datetime: raw data is st1=08, st2=00, sec=20, min=08, hr=10, mday=12, wday=25, mon=25, year=17
rtc-pcf8563 2-0051: pcf8563_get_datetime: tm is secs=20, mins=8, hours=10, mday=12, mon=4, year=117, wday=5
rtc-pcf8563 2-0051: pcf8563_rtc_read_alarm: raw data is min=44, hr=44, mday=52, wday=55
rtc-pcf8563 2-0051: pcf8563_rtc_read_alarm: tm is mins=44, hours=4, mday=12, wday=5, enabled=0, pending=0
rtc-pcf8563 2-0051: get_datetime.go
rtc-pcf8563 2-0051: pcf8563_get_datetime: raw data is st1=08, st2=00, sec=20, min=08, hr=10, mday=12, wday=25, mon=25, year=17
rtc-pcf8563 2-0051: pcf8563_get_datetime: tm is secs=20, mins=8, hours=10, mday=12, mon=4, year=117, wday=5
using rtc device, rtc-pcf8563, for alarms
rtc-pcf8563 2-0051: rtc core: registered rtc-pcf8563 as rtc0
i2c /dev entries driver
Linux video capture interface: v2.00
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16
mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17
usbcore: registered new interface driver uvcvideo
USB Video Class driver (v1.1.0)
imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
mmc0: SDHCI controller on platform [sdhci-esdhc-imx.3] using ADMA
sdhci sdhci-esdhc-imx.2: no write-protect pin available!
sdhci sdhci-esdhc-imx.2: no card-detect pin available!
mmc1: SDHCI controller on platform [sdhci-esdhc-imx.2] using ADMA
sdhci sdhci-esdhc-imx.0: no write-protect pin available!
sdhci sdhci-esdhc-imx.0: no card-detect pin available!
mmc2: SDHCI controller on platform [sdhci-esdhc-imx.0] using ADMA
mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
VPU initialized
mxc_asrc registered
Galcore version 4.6.9.9754
Thermal calibration data is 0x59550469
Thermal sensor with ratio = 185
Anatop Thermal registered as thermal_zone0
anatop_thermal_probe: default cooling device is cpufreq!
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
logger: created 256K log 'log_main'
logger: created 256K log 'log_events'
mmc0: new high speed DDR MMC card at address 0001
mmcblk0: mmc0:0001 4FPD3R 3.64 GiB
logger: created 256K log 'log_radio'
mmcblk0boot0: mmc0:0001 4FPD3R partition 1 4.00 MiB
mmcblk0boot1: mmc0:0001 4FPD3R partition 2 4.00 MiB
logger: created 256K log 'log_system'
mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4
mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio
imx-hdmi-soc-dai imx-hdmi-soc-dai.0: Failed: Load HDMI-video first.
sgtl5000 2-000a: Device with ID register 0 is not a sgtl5000
sgtl5000 2-000a: asoc: failed to probe CODEC sgtl5000.2-000a: -19
asoc: failed to instantiate card sgtl5000-audio: -19
Initialize HDMI-audio failed. Load HDMI-video first!
ALSA device list:
No soundcards found.
oprofile: using arm/armv7-ca9
u32 classifier
mmcblk0: p4 size 5455872 extends beyond EOD, truncated
Actions configured
Netfilter messages via NETLINK v0.30.
nf_conntrack version 0.5.0 (12474 buckets, 49896 max)
ctnetlink v0.93: registering with nfnetlink.
NF_TPROXY: Transparent proxy support initialized, version 4.1.0
NF_TPROXY: Copyright (c) 2006-2007 BalaBit IT Ltd.
xt_time: kernel timezone is -0000
mmcblk0boot1: unknown partition table
ip_tables: (C) 2000-2006 Netfilter Core Team
arp_tables: (C) 2002 David S. Miller
TCP cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 10
Mobile IPv6
ip6_tables: (C) 2000-2006 Netfilter Core Team
mmcblk0boot0: unknown partition table
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20090105 abi 8)
NET: Registered protocol family 29
can: raw protocol (rev 20090105)
can: broadcast manager protocol (rev 20090105 t)
lib80211: common routines for IEEE802.11 drivers
lib80211_crypt: registered algorithm 'NULL'
lib80211_crypt: registered algorithm 'WEP'
lib80211_crypt: registered algorithm 'CCMP'
lib80211_crypt: registered algorithm 'TKIP'
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Bus freq driver module loaded
Bus freq driver Enabled
mxc_dvfs_core_probe
DVFS driver module loaded
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
regulator_init_complete: VDDD: incomplete constraints, leaving on
regulator_init_complete: VDDIO: incomplete constraints, leaving on
regulator_init_complete: VDDA: incomplete constraints, leaving on
rtc-pcf8563 2-0051: get_datetime.go
rtc-pcf8563 2-0051: pcf8563_get_datetime: raw data is st1=08, st2=00, sec=20, min=08, hr=10, mday=12, wday=25, mon=25, year=17
rtc-pcf8563 2-0051: pcf8563_get_datetime: tm is secs=20, mins=8, hours=10, mday=12, mon=4, year=117, wday=5
rtc-pcf8563 2-0051: setting system clock to 2017-05-12 10:08:20 UTC (1494583700)
Freeing init memory: 248K

type=1400 audit(1494579405.040:4): avc: denied { entrypoint } for pid=1449 comm="init" path="/sbin/healthd" dev=rootfs ino=1478 scontext=u:r:healthd:s0 tcontext=u:object_r:rootfs:s0 tclass=file
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
init: watchdogd: Failed to open /dev/watchdog: No such file or directory
type=1400 audit(1494579405.070:5): avc: denied { read write } for pid=1458 comm="app_process" path=2F6465762F5F5F6E756C6C5F5F202864656C6574656429 dev=tmpfs ino=3082 scontext=u:r:zygote:s0 tcontext=u:object_r:tmpfs:s0 tclass=chr_file
healthd: wakealarm_init: timerfd_create failed
/system/bin/sh: No controlling tttype=1400 audit(1494579405.100:6): avc: denied { read write } for pid=1458 comm="app_process" path=2F6465762F5F5F6E756C6C5F5F202864656C6574656429 dev=tmpfs ino=3082 scontey: open /dev/tty: No such file orxt=u:r:zygote:s0 tcontext=u:object_r:tmpfs:s0 tclass=chr_file
directorytype=1400 audit(1494579405.110:7): avc: denied { read write } for pid=1462 comm="installd" path=2F6465762F5F5F6E756C6C5F5F202864656C6574656429 dev=tmpfs ino=3082 scontext=u:r:installd:s0 tcontext=u:object_r:tmpfs:s0 tclass=chr_file
type=1400 audit(1494579405.110:8): avc: denied { read write } for pid=1462 comm="installd" path=2F6465762F5F5F6E756C6C5F5F202864656C6574656429 dev=tmpfs ino=3082 scontext=u:r:installd:s0 tcontext=u:object_r:tmpfs:s0 tclass=chr_file
type=1400 audit(1494579405.110:9): avc: denied { read write } for pid=1462 comm="installd" path=2F6465762F5F5F6E756C6C5F5F202864656C6574656429 dev=tmpfs ino=3082 scontext=u:r:installd:s0 tcontext=u:object_r:tmpfs:s0 tclass=chr_file

/system/bin/sh: warning: won't htype=1400 audit(1494579405.110:10): avc: denied { read write } for pid=1452 comm="vold" path=2F6465762F5F5F6E756C6C5F5F202864656C6574656429 dev=tmpfs ino=3082 scontext=u:r:vold:s0 tcontext=u:object_r:tmpfs:s0 tclass=chr_file
ave full job controltype=1400 audit(1494579405.110:11): avc: denied { read write } for pid=1452 comm="vold" path=2F6465762F5F5F6E756C6C5F5F202864656C6574656429 dev=tmpfs ino=3082 scontext=u:r:vold:s0 tcontext=u:object_r:tmpfs:s0 tclass=chr_file
type=1400 audit(1494579405.110:12): avc: denied { read write } for pid=1452 comm="vold" path=2F6465762F5F5F6E756C6C5F5F202864656C6574656429 dev=tmpfs ino=3082 scontext=u:r:vold:s0 tcontext=u:object_r:tmpfs:s0 tclass=chr_file

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
init: property 'ro.serialno' doesn't exist while expanding '$ro.serialno'
init: cannot expand '$ro.serialno' while writing to '/sys/class/android_usb/android0/iSerial'
init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
root@sabresd_6dq:/ # init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
type=1400 audit(1494579405.300:13): avc: denied { read write } for pid=1458 comm="app_process" path=2F6465762F5F5F6E756C6C5F5F202864656C6574656429 dev=tmpfs ino=3082 scontext=u:r:zygote:s0 tcontext=u:object_r:tmpfs:s0 tclass=chr_file
Unable to handle kernel NULL pointer dereference at virtual address 00000019
request_suspend_state: wakeup (3->0) at 12670464337 (2017-05-12 08:56:45.343034001 UTC)
init: property 'sys.powerctl' doesn't exist while expanding '${sys.powerctl}'
init: powerctl: cannot expand '${sys.powerctl}'
init: property 'sys.sysctl.extra_free_kbytes' doesn't exist while expanding '${sys.sysctl.extra_free_kbytes}'
init: cannot expand '${sys.sysctl.extra_free_kbytes}' while writing to '/proc/sys/vm/extra_free_kbytes'
android_usb: already disabled
mtp_bind_config
adb_bind_config
pgd = d6920000
[00000019] *pgd=00000000
Internal error: Oops: 1 [#2] PREEMPT SMP
Modules linked in:
CPU: 1 Tainted: G D (3.0.35-gccd8e37 #69)
PC is at disk_part_iter_next+0x70/0xd8
LR is at 0x0
pc : [<c02d9b34>] lr : [<00000000>] psr: 200f0013
sp : d6683e68 ip : 00000000 fp : d60163e0
r10: c07f51dc r9 : d6278000 r8 : d660c068
r7 : 00000000 r6 : 00000001 r5 : d6683e80 r4 : 00000011
r3 : 00000008 r2 : d660c000 r1 : 00000004 r0 : d67fa2c0
Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
Control: 10c53c7d Table: 2692004a DAC: 00000015

PC: 0xc02d9ab4:
9ab4 c08f6850 c09a2c08 c07f4624 c07f45f4cyttsp5_core_rt_resume
e92d41f0 e1a05000 e5900004 e3500000
9ad4 0a000001 e2800020 eb01bd4b e3a03000 e5853004 ebf7fac5 e595300c e5952000
9af4 e3130001 e5920038 0a000023 e213c00c 13e0c000 03e06000 11a0600c e5951008
9b14 e151000c 1203e002 12037008 0a000010 e2813004 e7904103 e3540000 0a000008
9b34 e1c420d8 e1928003 1a00000c e35e0000 1a00000a e3570000 0a000001 e3510000
9b54 0a000006 e0811006 e5851008 e15c0001 1affffee ebf7fd87 e5950004 e8bd81f0
9b74 e2840020 eb01bd0f e5953008 e5854004 e0836006 e5856008 eafffff5 e590c008
9b94 e3a06001 eaffffdc e92d4070 e2403060 e24dd010 e1a06001 e3a02000 e1a01003

SP: 0xd6683de8:
3de8 c0dae380 c0dae380 00000001 012a8000 00000000 c00fe850 00000041 00000000
3e08 0000040f 00000001 00000001 00000000 d660c068 c004c550 d67fa2c0 00000004
3e28 d660c000 00000008 00000011 d6683e80 00000001 00000000 d660c068 d6278000
3e48 c07f51dc d60163e0 00000000 d6683e68 00000000 c02d9b34 200f0013 ffffffff
3e68 00000000 d6278000 d6278000 d660c060 d660c068 c02d9bd0 d660c000 00000000
3e88 00000004 00000000 d660c068 d6278000 00000000 c034aa6c d60163e0 c02e5ab8
3ea8 00000000 00000000 00000000 c034a98c 00000000 c06b74cc c0942338 c02e5de0
3ec8 00000000 d6683f78 00000001 d64f4000 0000000a 00000000 c07cf984 d682a2a0

FP: 0xd6016360:
6360 d6001380 d6016364 d6016364 d60163a0 00000000 c0901f04 d6022368 00000001
6380 00000003 00000000 00000000 00000000 00000000 00000000 00000000 00000000
63a0 d60013c0 d60163a4 d60163a4 00000000 00000000 c0901f04 d6022398 00000003
63c0 00000003 00000000 00000000 00000000 00000000 00000000 00000000 00000000
63e0 c0904c94 d6823414 00000000 00000000 d6001400 d60163f4 d60163f4 00000000
6400 00000000 c0901f18 d60223c8 00000377 00000003 c06b74cc 00000000 00000000
6420 d6043200 0000001e 00000005 00000003 00000002 00000050 00000001 00000000
6440 00000000 d6016444 d6016444 00000000 d6016450 d6016450 00000000 00000000

R0: 0xd67fa240:
a240 71797474 5f6f0065 72756f73 00006563 00000000 00000000 d67fb9c8 c00b18dc
a260 73627573 65747379 0000006d 00000000 00000000 00000000 00000000 00000000
a280 30333a33 73650000 7269762f 6c617574 7974742f 7974742f 00003171 00000000
a2a0 71797474 00000065 00000000 00000000 00000000 00000000 00000000 00000000
a2c0 00000000 00000000 00000000 00000000 d660c040 00000000 00000000 00000000
a2e0 00000011 00000000 00000000 00000000 00000000 00000000 00000000 00000000
a300 6e756f6d 006e6f74 00000000 00000000 00000000 00000000 00000000 00000000
a320 71797474 73650065 7269762f 6c617574 7974742f 7974742f 00006471 00000000

R2: 0xd660bf80:
bf80 c00ab278 d660a000 00000000 00000000 00000000 c0343040 00000000 00000000
bfa0 d6351520 c00ab278 c09048a8 c09048a8 d602ff4c 00000000 c0342f30 00000013
bfc0 00000000 c00aab1c c004d6a8 00000000 00000000 00000000 00000000 00000000
bfe0 d660bfe0 d660bfe0 d602ff4c c00aaa9c c004d6a8 c004d6a8 00000000 00000000
c000 000000b3 00000010 00000008 62636d6d 62306b6c 31746f6f 00000000 00000000
c020 00000000 00000000 00000000 00000000 00000000 00000000 d67fa2c0 00000000
c040 00000000 00000000 00002000 00000000 00000000 00000000 00000000 00000000
c060 d65bd860 d6781da0 d67f3f60 d697d20c d697d40c d65bd868 d60163e0 c0904ae0

R5: 0xd6683e00:
3e00 00000041 00000000 0000040f 00000001 00000001 00000000 d660c068 c004c550
3e20 d67fa2c0 00000004 d660c000 00000008 00000011 d6683e80 00000001 00000000
3e40 d660c068 d6278000 c07f51dc d60163e0 00000000 d6683e68 00000000 c02d9b34
3e60 200f0013 ffffffff 00000000 d6278000 d6278000 d660c060 d660c068 c02d9bd0
3e80 d660c000 00000000 00000004 00000000 d660c068 d6278000 00000000 c034aa6c
3ea0 d60163e0 c02e5ab8 00000000 00000000 00000000 c034a98c 00000000 c06b74cc
3ec0 c0942338 c02e5de0 00000000 d6683f78 00000001 d64f4000 0000000a 00000000
3ee0 c07cf984 d682a2a0 4003315c c013e38c c029ef68 d661a720 00000002 00000004

R8: 0xd660bfe8:
bfe8 d602ff4c c00aaa9c c004d6a8 c004d6a8 00000000 00000000 000000b3 00000010
c008 00000008 62636d6d 62306b6c 31746f6f 00000000 00000000 00000000 00000000
c028 00000000 00000000 00000000 00000000 d67fa2c0 00000000 00000000 00000000
c048 00002000 00000000 00000000 00000000 00000000 00000000 d65bd860 d6781da0
c068 d67f3f60 d697d20c d697d40c d65bd868 d60163e0 c0904ae0 d697b908 00000007
c088 00000007 00000000 c0901b34 00000001 00000000 00000000 d660c0a0 d660c0a0
c0a8 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
c0c8 d697d268 d697d468 7fffffff 00000000 00000000 d660c0dc d660c0dc 00000000

R9: 0xd6277f80:
7f80 260e4811 260e4c11 260e5811 260e5c11 260e6811 260e6c11 260e7811 260e7c11
7fa0 260e8811 260e8c11 260e9811 260e9c11 260ea811 260eac11 260eb811 260ebc11
7fc0 260ec811 260ecc11 260ed811 260edc11 260ee811 260eec11 260ef811 260efc11
7fe0 260f0811 260f0c11 260f1811 260f1c11 260f2811 260f2c11 28ffe821 28ffec21
8000 d6278084 d627808f d62780ee d62780fe d6278108 d6278111 d6278126 00000000
8020 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
8040 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
8060 00000000 00000000 00000000 00000000 00000000 00000000 00000000
cyttsp5_i2c_adapter 1-0024: cyttsp5_hid_exec_cmd_and_wait_: HID output cmd execution timed out
cyttsp5_i2c_adapter 1-0024: cyttsp5_hid_cmd_set_power_: Failed to set power to state:0
00000000

R10: 0xc07f515c:
515c 00000a21 49544341 253d4e4f 00000073 50564544 3d485441 00007325 53425553
517c 45545359 73253d4d
cyttsp5_i2c_adapter 1-0024: cyttsp5_core_rt_resume: Error on wake
00000000 6a626f6b 3a746365 73252720 25282027 203a2970
519c 203a7325 65766575 2928746e 74657220 656e7275 64252064 0000000a 4e514553
51bc 253d4d55 00756c6c 25407325 00000073 6a626f6b 5f746365 65766575 0000746e
51dc 00646461 6f6d6572 00006576 6e616863 00006567 65766f6d 00000000 696c6e6f
51fc 0000656e 6c66666f 00656e69 2f62696c 6665726b 0000632e 2f62696c 73696c70
521c 00632e74 2f62696c 6f697270 6572745f 00632e65 2d647026 74756d3e 00007865
523c 2f62696c 69646172 72742d78 632e6565 00000000 69646172 72745f78 6e5f6565
Process vold (pid: 1452, stack limit = 0xd66822f0)
Stack: (0xd6683e68 to 0xd6684000)
3e60: 00000000 d6278000 d6278000 d660c060 d660c068 c02d9bd0
3e80: d660c000 00000000 00000004 00000000 d660c068 d6278000 00000000 c034aa6c
3ea0: d60163e0 c02e5ab8 00000000 00000000 00000000 c034a98c 00000000 c06b74cc
3ec0: c0942338 c02e5de0 00000000 d6683f78 00000001 d64f4000 0000000a 00000000
3ee0: c07cf984 d682a2a0 4003315c c013e38c c029ef68 d661a720 00000002 00000004
3f00: d660c060 d69739f8 d6683f88 c06b74e8 d660c068 d697b8d8 4003315c c03499a8
3f20: d6683f88 00000000 00000004 00000004 d69739e0 c0348f0c 00000004 c01816f4
3f40: d661a720 00000004 4002c247 d6683f88 00000004 d6682000 00000000 c0130cfc
3f60: 00000001 c0132368 00000000 00000000 d661a720 4002c247 00000004 c0130f88
3f80: 00000022 00000001 00000000 00000000 00000002 0000000b 0000000a 00000004
3fa0: c004cd04 c004cb80 00000002 0000000b 0000000b 4002c247 00000004 00000001
3fc0: 00000002 0000000b 0000000a 00000004 41bdefc0 0000000a 4003315c 4003315c
3fe0: 41bdefc0 bed42850 4001ec63 401be3c0 200f0010 0000000b 00000000 00000000
[<c02d9b34>] (disk_part_iter_next+0x70/0xd8) from [<c02d9bd0>] (disk_uevent+0x34/0x64)
[<c02d9bd0>] (disk_uevent+0x34/0x64) from [<c034aa6c>] (dev_uevent+0xe0/0x248)
[<c034aa6c>] (dev_uevent+0xe0/0x248) from [<c02e5de0>] (kobject_uevent_env+0x254/0x5bc)
[<c02e5de0>] (kobject_uevent_env+0x254/0x5bc) from [<c03499a8>] (store_uevent+0x4c/0x54)
[<c03499a8>] (store_uevent+0x4c/0x54) from [<c0348f0c>] (dev_attr_store+0x18/0x24)
[<c0348f0c>] (dev_attr_store+0x18/0x24) from [<c01816f4>] (sysfs_write_file+0x168/0x198)
[<c01816f4>] (sysfs_write_file+0x168/0x198) from [<c0130cfc>] (vfs_write+0xa0/0x144)
[<c0130cfc>] (vfs_write+0xa0/0x144) from [<c0130f88>] (sys_write+0x38/0x70)
[<c0130f88>] (sys_write+0x38/0x70) from [<c004cb80>] (ret_fast_syscall+0x0/0x30)
Code: e2813004 e7904103 e3540000 0a000008 (e1c420d8)
---[ end trace 72ffca938b1f1a4b ]---
Kernel panic - not syncing: Fatal exception
[<c00541a0>] (unwind_backtrace+0x0/0x138) from [<c067a330>] (panic+0x74/0x198)
[<c067a330>] (panic+0x74/0x198) from [<c00506f8>] (die+0x220/0x28c)
[<c00506f8>] (die+0x220/0x28c) from [<c0679574>] (__do_kernel_fault.part.3+0x54/0x74)
[<c0679574>] (__do_kernel_fault.part.3+0x54/0x74) from [<c0058034>] (do_translation_fault+0x0/0xa0)
[<c0058034>] (do_translation_fault+0x0/0xa0) from [<c02d9b34>] (disk_part_iter_next+0x70/0xd8)
[<c02d9b34>] (disk_part_iter_next+0x70/0xd8) from [<00040257>] (0x40257)
CPU0: stopping
[<c00541a0>] (unwind_backtrace+0x0/0x138) from [<c004639c>] (do_IPI+0x188/0x1bc)
[<c004639c>] (do_IPI+0x188/0x1bc) from [<c004c5cc>] (__irq_svc+0x4c/0xe8)
Exception stack(0xc08bff68 to 0xc08bffb0)
ff60: c09564c8 20000093 00000001 00000000 c08be000 c094df64
ff80: c08d3a70 c0684a90 c08dc29c 412fc09a 00000000 00000000 00000000 c08bffb0
ffa0: c005c354 c004d708 40000013 ffffffff
[<c004c5cc>] (__irq_svc+0x4c/0xe8) from [<c004d708>] (default_idle+0x24/0x28)
[<c004d708>] (default_idle+0x24/0x28) from [<c004d9f8>] (cpu_idle+0xac/0x120)
[<c004d9f8>] (cpu_idle+0xac/0x120) from [<c00088c8>] (start_kernel+0x2a0/0x2f0)
[<c00088c8>] (start_kernel+0x2a0/0x2f0) from [<10008040>] (0x10008040)

标签 (1)
0 项奖励
回复
1 回复

1,136 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jack

please check that wdog signal reset also pmic (using pwron signal) as it is

done on Sabre SD schematic spf-27392 p.21, U507. Otherwise some peripherals may be not

reset properly and various issues may be happen

Schematics (1)
i.MX6_SABRE_SDP_DESIGNFILES
http://www.nxp.com/products/software-and-tools/hardware-development-tools/sabre-development-system/s...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复