imx6d can't work well when using two capture interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imx6d can't work well when using two capture interface

跳至解决方案
1,686 次查看
leihe
Contributor I

the single comes from ds90ub940 and adv7180 ,ds90ub940 config is ipu0、csi1、VC1,adv7180 config is ipu0、csi0、VC0,if  ds90ub940's FPDlink is disconnected this two video will lost. this two video device can work well along .can somebody help me thank you.

标签 (6)
0 项奖励
回复
1 解答
1,474 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lei

may be helpful to look at several cameras example on

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,475 次查看
igorpadykov
NXP Employee
NXP Employee

Hi lei

may be helpful to look at several cameras example on

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------