imx6d camera device tree

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6d camera device tree

Jump to solution
2,446 Views
aaronpadilla
Contributor II

Hi,

I am trying to setup a RPi camera on my QWKS-SCMIMX6, the chip on camera is the IMX219 , the camera plugs directly on my board, I am using the yocto BSP,  I have checked the mxc-camera in menuconfig but the camera is not working and seems not to be in the device file, I have some experience remapping the DT for simplest devices such as GPIO and UART, but I did not found a related example as start point, actually I don't know were to start, could you advice?

Thanks in advance. 

0 Kudos
Reply
1 Solution
2,071 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aaron

one can look at imx6q-sabresd.dts

linux-2.6-imx.git - Freescale i.MX Linux Tree 

and Linux documentation in

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.0.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

use AN5305 MIPI-CSI2 Peripheral on i.MX6 MPU
http://cache.nxp.com/files/32bit/doc/app_note/AN5305.pdf
https://community.freescale.com/docs/DOC-94312

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,072 Views
igorpadykov
NXP Employee
NXP Employee

Hi Aaron

one can look at imx6q-sabresd.dts

linux-2.6-imx.git - Freescale i.MX Linux Tree 

and Linux documentation in

http://www.nxp.com/webapp/Download?colCode=L4.1.15_1.0.0_LINUX_DOCS&Parent_nodeId=133769948107170617... 

use AN5305 MIPI-CSI2 Peripheral on i.MX6 MPU
http://cache.nxp.com/files/32bit/doc/app_note/AN5305.pdf
https://community.freescale.com/docs/DOC-94312

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply