imx6SL ethernet EMI problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6SL ethernet EMI problem

1,558件の閲覧回数
fisherhe
Contributor II

Hi,

   I use imx6sololite and the ethernet topology is as blows:

pastedImage_1.png 

      Now there is EMI problem on ethernet coming from the clock(FEC_REF_CLK). Then  I set the SRE of this pad to slow, but it has no help.

      Is there any other metholds to decrease the EMI coming out of the ethernet clock.Will setting DSE bit useful?or other metholds suggested?

      Many thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

1,532件の閲覧回数
Yuri
NXP Employee
NXP Employee

fisherhe 

Hello,

   The DSE bit field (drive strength) affects EMI environment.

The similar result may be achieved if use series resistor.

Regards,

Yuri.