imx6SL LPDDR2 Script Aid -64MB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6SL LPDDR2 Script Aid -64MB

1,706件の閲覧回数
thejay
NXP Employee
NXP Employee

Our customer is using the imx6SL and 64MB of LPDDR2. MT42L16M32D1AC-25 IT:A which is a 512Mbit, 4 Meg x 32x 4 banks part.

The LPDDR2 script aid only goes down to 2GB.

Is there any easy way to modify the script or calcualte the DDR register values?

Thanks,

Jay

ラベル(1)
0 件の賞賛
返信
1 返信

1,416件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello John Marcinczyk,

Unfortunately the usual script aid goes only to 2Gb, which would be 256MB and it’s still much over 64MB.

Have you tried using the newest version on the following link? It uses Gb as unit but you can enter decimal numbers.

https://community.freescale.com/docs/DOC-105968

At least it shows more information on the registers so it may help to see which ones would be affected so I hope it helps.

0 件の賞賛
返信