imx6DL board add the logo patch GPU has some problem on android 5.0 platform.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6DL board add the logo patch GPU has some problem on android 5.0 platform.

1,971 Views
尚飞汤
Contributor IV

The error is as below:

=~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2015.12.14 19:12:15 =~=~=~=~=~=~=~=~=~=~=~=

    1     0

gpio1 value = 80cc

gpio1 value = 80cc

gpio1 value = 80cc

BQ27541 probe OK !

BQ27541: Device type is 0x0541

Battery[1]: voltage = 3961 mV, current = -721 mA

           capacity =   89 %, charge = 4445 mAH, temperature =  21 C

Battery[2]: voltage = 3961 mV, current = -721 mA,

capacity =   89 %, charge = 4445 mAH, temperature =  21 C

cond: voltage = 3961, capacity = 89 can start to boot..

check boot mode start!!

booti mmc1

kernel   @ 14008000 (6768480)

ramdisk  @ 15000000 (895546)

fdt      @ 14f00000 (58314)

get_ftd_mode = 0

kernel cmdline:

use boot.img command line:

console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,if=RGB24,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmem=14M gpumem=128M vmalloc=400M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M fb0base=0x27b00000 androidboot.selinux=permissive androidboot.dm_verity=disabled androidboot.serialno=0c1e69d4df6518db

Using Device Tree in place at 14f00000, end 14f113c9

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0

[    0.000000] Initializing cgroup subsys cpu

[    0.000000] Initializing cgroup subsys cpuacct

[    0.000000] Linux version 3.10.53 (aaron@bp153) (gcc version 4.6.x-google 20120106 (prerelease) (GCC) ) #13 SMP PREEMPT Mon Dec 14 19:03:27 CST 2015

[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

[    0.000000] Machine: Freescale i.MX6 Quad/DualLite (Device Tree), model: Freescale i.MX6 DualLite SABRE Smart Device Board(EM70)

[    0.000000] cma: CMA: failed to reserve 384 MiB

[    0.000000] Memory policy: ECC disabled, Data cache writealloc

[    0.000000] PERCPU: Embedded 8 pages/cpu @c1491000 s9856 r8192 d14720 u32768

[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 257088

[    0.000000] Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,if=RGB24,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off fbmem=14M gpumem=128M vmalloc=400M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=384M fb0base=0x27b00000 androidboot.selinux=permissive androidboot.dm_verity=disabled androidboot.serialno=0c1e69d4df6518db

[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)

[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

[    0.000000] Memory: 379MB 566MB 64MB = 1009MB total

[    0.000000] Memory: 1010280k/1010280k available, 38296k reserved, 424960K highmem

[    0.000000] Virtual kernel memory layout:

[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)

[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

[    0.000000]     vmalloc : 0xe6800000 - 0xff000000   ( 392 MB)

[    0.000000]     lowmem  : 0xc0000000 - 0xe6000000   ( 608 MB)

[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)

[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)

[    0.000000]       .text : 0xc0008000 - 0xc0b07290   (11261 kB)

[    0.000000]       .init : 0xc0b08000 - 0xc0b56680   ( 314 kB)

[    0.000000]       .data : 0xc0b58000 - 0xc0be0000   ( 544 kB)

[    0.000000]        .bss : 0xc0be0000 - 0xc0c74978   ( 595 kB)

[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1

[    0.000000] Preemptible hierarchical RCU implementation.

[    0.00000 80 e20b5e88 e20b5e88 e23b0500 00000000 00000001 00000000

[    4.691230] 5ea0  00000000 00000000 5f757076 00007177 00000000 00000000 00000000 00000000

[    4.699590]

[    4.699590] FP: 0xe2482984:

[    4.703869] 2984  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.712226] 29a4  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.720582] 29c4  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.728937] 29e4  00000000 00000000 00000000 00000000 00000000 00000000 00000000 e23e0000

[    4.737293] 2a04  00000000 00000000 00000000 c0c4ed58 00000000 00000000 00000000 00000000

[    4.745649] 2a24  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.754005] 2a44  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.762363] 2a64  e69f8000 e6ac8000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.770721]

[    4.770721] R0: 0xc00e1d68:

[    4.774999] 1d68  e250a000 0a000005 e1a00005 e1a0100a eb073a99 e2509000 1afffff1 eaffffc4

[    4.783360] 1d88  e3e0800b eaffffe7 e1a0a005 eaffffc0 e59f0040 e3001458 ebfd2f43 eaffffcf

[    4.791718] 1da8  e59f0030 e3001457 ebfd2f3f e59630d4 eaffffc7 e7f001f2 e5973000 e3001466

[    4.800074] 1dc8  e59f0010 e59f2010 e1cd40f0 ebfd2f4f eaffffcf c0b71aa8 c09d95a8 c09d970c

[    4.808434] 1de8  e1a00002 e12fff1e e92d4038 e1a05000 e5904024 e3540000 0a000004 e1a00004

[    4.816792] 1e08  ebfe57c7 e3500000 01a05000 0a000003 e1a00005 eb08bc5b e2505000 0a000001

[    4.825148] 1e28  e1a00005 e8bd8038 e1a00004 ebfe57ec eafffffa e92d4008 e1a00001 ebffffe9

[    4.833505] 1e48  e3500000 03e00000 13a00000 e8bd8008 e92d4010 e1a04000 e59f0040 eb1c917b

[    4.841867]

[    4.841867] R4: 0xc00e1d68:

[    4.846146] 1d68  e250a000 0a000005 e1a00005 e1a0100a eb073a99 e2509000 1afffff1 eaffffc4

[    4.854504] 1d88  e3e0800b eaffffe7 e1a0a005 eaffffc0 e59f0040 e3001458 ebfd2f43 eaffffcf

[    4.862864] 1da8  e59f0030 e3001457 ebfd2f3f e59630d4 eaffffc7 e7f001f2 e5973000 e3001466

[    4.871220] 1dc8  e59f0010 e59f2010 e1cd40f0 ebfd2f4f eaffffcf c0b71aa8 c09d95a8 c09d970c

[    4.879578] 1de8  e1a00002 e12fff1e e92d4038 e1a05000 e5904024 e3540000 0a000004 e1a00004

[    4.887936] 1e08  ebfe57c7 e3500000 01a05000 0a000003 e1a00005 eb08bc5b e2505000 0a000001

[    4.896293] 1e28  e1a00005 e8bd8038 e1a00004 ebfe57ec eafffffa e92d4008 e1a00001 ebffffe9

[    4.904648] 1e48  e3500000 03e00000 13a00000 e8bd8008 e92d4010 e1a04000 e59f0040 eb1c917b

[    4.913004]

[    4.913004] R5: 0xe23dff80:

[    4.917283] ff80  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.925641] ffa0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.933996] ffc0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.942351] ffe0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.950707] 0000  2020534f e2482a00 e23f7240 e23f7280 00000000 00000000 00000001 e23f7300

[    4.959065] 0020  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    4.967420] 0040  00000000 e23f7340 00000000 00000000 00000000 00000000 00000000 00000000

[    4.975778] 0060  00000000 00000000 00000000 00000000 e23f72c0 e23e0100 c143fe40 00000010

[    4.984136]

[    4.984136] R7: 0xc0c76ba0:

[    4.988414] 6ba0  00000400 00000000 00000000 ffffffff 00000001 c0c76bb4 c0c76bb4 00000000

[    4.996774] 6bc0  00000400 00000000 00000000 ffffffff 00000001 c0c76bd4 c0c76bd4 00000000

[    5.005133] 6be0  00000400 00000000 00000000 ffffffff 00000001 c0c76bf4 c0c76bf4 00000000

[    5.013491] 6c00  00000400 00000000 00000000 ffffffff 00000001 c0c76c14 c0c76c14 00000000

[    5.021848] 6c20  00000400 00000000 00000000 ffffffff 00000001 c0c76c34 c0c76c34 00000000

[    5.030207] 6c40  00000400 00000000 00000000 ffffffff 00000001 c0c76c54 c0c76c54 00000000

[    5.038564] 6c60  00000400 00000000 00000000 ffffffff 00000001 c0c76c74 c0c76c74 00000000

[    5.046921] 6c80  00000400 00000000 00000000 ffffffff 00000001 c0c76c94 c0c76c94 00000000

[    5.055281]

[    5.055281] R9: 0xe2482980:

[    5.059560] 2980  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    5.067917] 29a0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    5.076274] 29c0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    5.084629] 29e0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    5.092985] 2a00  e23e0000 00000000 00000000 00000000 c0c4ed58 00000000 00000000 00000000

[    5.101341] 2a20  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    5.109701] 2a40  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    5.118060] 2a60  00000000 e69f8000 e6ac8000 00000000 00000000 00000000 00000000 00000000

[    5.126419] Process swapper/0 (pid: 1, stack limit = 0xe2074238)

[    5.132435] Stack: (0xe2075cd0 to 0xe2076000)

[    5.136804] 5cc0:                                     00000000 e23e0000 e23e0000 00000000

[    5.144995] 5ce0: fffffffd 00000000 e2482a00 00000000 e2482a04 c0585544 e23e0300 c0585588

[    5.153185] 5d00: 00000000 c05859c8 00000000 c058e440 00000000 e20b5d80 00000029 e2482a00

[    5.161375] 5d20: 00000000 e2482a0c 00000000 e2075df4 00000000 00000029 0000002a c0583f9c

[    5.169564] 5d40: e2482a04 e23f6f00 00000000 00000000 c0be2502 00000000 e23f6b80 e2482a00

[    5.177754] 5d60: 00000000 00000000 00000000 00000000 00000001 00000000 ffffffff c07fd5d4

[    5.185944] 5d80: c0a5b8ec c0bbeeec 00000000 e2137600 00000000 ffffffff 00000800 00000000

[    5.194133] 5da0: 00000030 c058c10c 00134000 00004000 ffffffff 00000000 00000800 00000000

[    5.202323] 5dc0: 08000000 00000000 ffffffff ffffffff 00000000 00000000 00000030 00000000

[    5.210511] 5de0: ffffffff 00000000 e2075df4 e2075df0 00000000 00000001 00000001 00000001

[    5.218700] 5e00: 00000000 c0c4ed58 00000001 00000029 00130000 00004000 0000002a 00134000

[    5.226891] 5e20: 00004000 ffffffff 00000000 00000800 08000000 00000000 00000000 00000000

[    5.235081] 5e40: ffffffff ffffffff ffffffff 00000000 00000030 00000000 00000000 00000000

[    5.243272] 5e60: 00000001 00000001 00000000 00000001 e2137610 c0c48294 e2137610 00000000

[    5.251463] 5e80: 00000000 c0bbef00 c0b53630 00000173 00000000 c039ecfc c039ece4 c039db4c

[    5.259653] 5ea0: 00000000 e2137610 c0bbef00 e2137644 00000000 00000000 00000173 c039dd8c

[    5.267842] 5ec0: c0bbef00 00000000 c039dd00 c039c340 e204285c e21274b4 c0bbef00 c0b88120

[    5.276032] 5ee0: e23f5280 c039d2bc c0a5b5e8 c0bbef00 c0bbef00 c0c4ed58 c0b4b2e8 c0b379c8

[    5.284222] 5f00: 00000000 c039e240 00000000 c0c4ed58 c0c4ed58 c0b37ab8 00000000 c0be0000

[    5.292410] 5f20: e2074000 c000864c 00000001 00000003 00000000 00000000 c148e641 c0049158

[    5.300600] 5f40: c0a3bbd8 c0ac4cf0 00000006 00000006 c0b6e644 c0b4b308 00000006 c0b4b2e8

[    5.308790] 5f60: c0be0000 c0b08428 c0b53630 00000173 00000000 c0b08b90 00000006 00000006

[    5.316980] 5f80: c0b08428 c0053b54 00000000 c07f86a4 00000000 00000000 00000000 00000000

[    5.325169] 5fa0: 00000000 c07f86ac 00000000 c000e0d8 00000000 00000000 00000000 00000000

[    5.333358] 5fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[    5.341547] 5fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000

[    5.349753] [<c00d9f7c>] (kfree+0x160/0x16c) from [<c0585544>] (gckOS_FreeMemory+0x48/0x7c)

[    5.358124] [<c0585544>] (gckOS_FreeMemory+0x48/0x7c) from [<c0585588>] (gckOS_Free+0x10/0x20)

[    5.366753] [<c0585588>] (gckOS_Free+0x10/0x20) from [<c05859c8>] (gckOS_DeleteMutex+0x10/0x20)

[    5.375471] [<c05859c8>] (gckOS_DeleteMutex+0x10/0x20) from [<c058e440>] (gckKERNEL_Construct+0x1f8/0x42c)

[    5.385143] [<c058e440>] (gckKERNEL_Construct+0x1f8/0x42c) from [<c0583f9c>] (gckGALDEVICE_Construct+0x178/0x9ac)

[    5.395420] [<c0583f9c>] (gckGALDEVICE_Construct+0x178/0x9ac) from [<c058c10c>] (gpu_probe+0x230/0x380)

[    5.404832] [<c058c10c>] (gpu_probe+0x230/0x380) from [<c039ecfc>] (platform_drv_probe+0x18/0x1c)

[    5.413728] [<c039ecfc>] (platform_drv_probe+0x18/0x1c) from [<c039db4c>] (driver_probe_device+0x8c/0x240)

[    5.423401] [<c039db4c>] (driver_probe_device+0x8c/0x240) from [<c039dd8c>] (__driver_attach+0x8c/0x90)

[    5.432811] [<c039dd8c>] (__driver_attach+0x8c/0x90) from [<c039c340>] (bus_for_each_dev+0x60/0x94)

[    5.441875] [<c039c340>] (bus_for_each_dev+0x60/0x94) from [<c039d2bc>] (bus_add_driver+0xd8/0x228)

[    5.450937] [<c039d2bc>] (bus_add_driver+0xd8/0x228) from [<c039e240>] (driver_register+0x78/0xf4)

[    5.459914] [<c039e240>] (driver_register+0x78/0xf4) from [<c0b37ab8>] (gpu_init+0xf0/0x12c)

[    5.468369] [<c0b37ab8>] (gpu_init+0xf0/0x12c) from [<c000864c>] (do_one_initcall+0xf4/0x154)

[    5.476913] [<c000864c>] (do_one_initcall+0xf4/0x154) from [<c0b08b90>] (kernel_init_freeable+0x100/0x1cc)

[    5.486590] [<c0b08b90>] (kernel_init_freeable+0x100/0x1cc) from [<c07f86ac>] (kernel_init+0x8/0xe4)

[    5.495744] [<c07f86ac>] (kernel_init+0x8/0xe4) from [<c000e0d8>] (ret_from_fork+0x14/0x3c)

[    5.504109] Code: e7933282 e3130902 11a07001 eaffffb6 (e7f001f2)

[    5.510232] ---[ end trace 8723c1d3b95be2d9 ]---

[    5.516830] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

[    5.516830]

[    5.516891] mmcblk2: mmc2:0001 MMC08G 7.20 GiB

[    5.517143] mmcblk2boot0: mmc2:0001 MMC08G partition 1 2.00 MiB

[    5.517384] mmcblk2boot1: mmc2:0001 MMC08G partition 2 2.00 MiB

[    5.517622] mmcblk2rpmb: mmc2:0001 MMC08G partition 3 128 KiB

[    5.548128] CPU0: stopping

[    5.550855] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G      D      3.10.53 #13

[    5.557934] [<c0013d48>] (unwind_backtrace+0x0/0xf8) from [<c0011868>] (show_stack+0x10/0x14)

[    5.566479] [<c0011868>] (show_stack+0x10/0x14) from [<c0012f94>] (handle_IPI+0x178/0x1a4)

[    5.574760] [<c0012f94>] (handle_IPI+0x178/0x1a4) from [<c00084c8>] (gic_handle_irq+0x54/0x5c)

[    5.583389] [<c00084c8>] (gic_handle_irq+0x54/0x5c) from [<c000dc40>] (__irq_svc+0x40/0x70)

[    5.591750] Exception stack(0xc0b59f78 to 0xc0b59fc0)

[    5.596813] 9f60:                                                       ffffffed 0093d000

[    5.605004] 9f80: c0b61b58 00000000 c0b58000 c0b605a8 c0809dec c0bdfeba c0bdfeba 412fc09a

[    5.613193] 9fa0: 00000001 00000000 00000000 c0b59fc0 c000ed58 c000ed48 60000113 ffffffff

[    5.621391] [<c000dc40>] (__irq_svc+0x40/0x70) from [<c000ed48>] (arch_cpu_idle+0x30/0x48)

[    5.629680] [<c000ed48>] (arch_cpu_idle+0x30/0x48) from [<c0067bb0>] (cpu_startup_entry+0x9c/0x138)

[    5.638746] [<c0067bb0>] (cpu_startup_entry+0x9c/0x138) from [<c0b08a38>] (start_kernel+0x2d4/0x32c)

[    5.647894] [<c0b08a38>] (start_kernel+0x2d4/0x32c) from [<10008074>] (0x10008074)

[    5.657389] ------------[ cut here ]------------

[    5.662032] WARNING: at /home/aaron/work_space/em_new/imx6lp/kernel_imx/kernel/smp.c:382 smp_call_function_many+0xc8/0x2e4()

[    5.673256] Modules linked in:

[    5.676343] CPU: 1 PID: 1 Comm: swapper/0 Tainted: G      D      3.10.53 #13

[    5.683412] [<c0013d48>] (unwind_backtrace+0x0/0xf8) from [<c0011868>] (show_stack+0x10/0x14)

[    5.691956] [<c0011868>] (show_stack+0x10/0x14) from [<c002da98>] (warn_slowpath_common+0x4c/0x68)

[    5.700932] [<c002da98>] (warn_slowpath_common+0x4c/0x68) from [<c002dad0>] (warn_slowpath_null+0x1c/0x24)

[    5.710603] [<c002dad0>] (warn_slowpath_null+0x1c/0x24) from [<c0075fc8>] (smp_call_function_many+0xc8/0x2e4)

[    5.720536] [<c0075fc8>] (smp_call_function_many+0xc8/0x2e4) from [<c0076378>] (smp_call_function+0x34/0x68)

[    5.730377] [<c0076378>] (smp_call_function+0x34/0x68) from [<c00763ec>] (on_each_cpu+0x28/0x70)

[    5.739181] [<c00763ec>] (on_each_cpu+0x28/0x70) from [<c07fd454>] (panic+0xb0/0x1fc)

[    5.747032] [<c07fd454>] (panic+0xb0/0x1fc) from [<c0032dd8>] (do_exit+0x79c/0x8b4)

[    5.754705] [<c0032dd8>] (do_exit+0x79c/0x8b4) from [<c0011a58>] (die+0x1ec/0x3a8)

[    5.762288] [<c0011a58>] (die+0x1ec/0x3a8) from [<c0008250>] (do_undefinstr+0x8c/0x174)

[    5.770308] [<c0008250>] (do_undefinstr+0x8c/0x174) from [<c000dcec>] (__und_svc_finish+0x0/0x14)

[    5.779189] Exception stack(0xe2075c88 to 0xe2075cd0)

[    5.784254] 5c80:                   c00e1de8 00000400 000000e1 00000400 c00e1de8 e23e0000

[    5.792445] 5ca0: 00000000 c0c76c20 00000000 e2482a00 00000000 e2482a04 e20b5e40 e2075cd0

[    5.800635] 5cc0: c0585544 c00d9f7c 40000113 ffffffff

[    5.805707] [<c000dcec>] (__und_svc_finish+0x0/0x14) from [<c00d9f7c>] (kfree+0x160/0x16c)

[    5.813994] [<c00d9f7c>] (kfree+0x160/0x16c) from [<c0585544>] (gckOS_FreeMemory+0x48/0x7c)

[    5.822361] [<c0585544>] (gckOS_FreeMemory+0x48/0x7c) from [<c0585588>] (gckOS_Free+0x10/0x20)

[    5.830990] [<c0585588>] (gckOS_Free+0x10/0x20) from [<c05859c8>] (gckOS_DeleteMutex+0x10/0x20)

[    5.839707] [<c05859c8>] (gckOS_DeleteMutex+0x10/0x20) from [<c058e440>] (gckKERNEL_Construct+0x1f8/0x42c)

[    5.849376] [<c058e440>] (gckKERNEL_Construct+0x1f8/0x42c) from [<c0583f9c>] (gckGALDEVICE_Construct+0x178/0x9ac)

[    5.859653] [<c0583f9c>] (gckGALDEVICE_Construct+0x178/0x9ac) from [<c058c10c>] (gpu_probe+0x230/0x380)

[    5.869064] [<c058c10c>] (gpu_probe+0x230/0x380) from [<c039ecfc>] (platform_drv_probe+0x18/0x1c)

[    5.877958] [<c039ecfc>] (platform_drv_probe+0x18/0x1c) from [<c039db4c>] (driver_probe_device+0x8c/0x240)

[    5.887630] [<c039db4c>] (driver_probe_device+0x8c/0x240) from [<c039dd8c>] (__driver_attach+0x8c/0x90)

[    5.897040] [<c039dd8c>] (__driver_attach+0x8c/0x90) from [<c039c340>] (bus_for_each_dev+0x60/0x94)

[    5.906104] [<c039c340>] (bus_for_each_dev+0x60/0x94) from [<c039d2bc>] (bus_add_driver+0xd8/0x228)

[    5.915167] [<c039d2bc>] (bus_add_driver+0xd8/0x228) from [<c039e240>] (driver_register+0x78/0xf4)

[    5.924143] [<c039e240>] (driver_register+0x78/0xf4) from [<c0b37ab8>] (gpu_init+0xf0/0x12c)

[    5.932596] [<c0b37ab8>] (gpu_init+0xf0/0x12c) from [<c000864c>] (do_one_initcall+0xf4/0x154)

[    5.941137] [<c000864c>] (do_one_initcall+0xf4/0x154) from [<c0b08b90>] (kernel_init_freeable+0x100/0x1cc)

[    5.950811] [<c0b08b90>] (kernel_init_freeable+0x100/0x1cc) from [<c07f86ac>] (kernel_init+0x8/0xe4)

[    5.959961] [<c07f86ac>] (kernel_init+0x8/0xe4) from [<c000e0d8>] (ret_from_fork+0x14/0x3c)

[    5.968321] ---[ end trace 8723c1d3b95be2da ]---

[    5.973357] Rebooting in 5 seconds..

can someone tell me how is that going???

Labels (4)
0 Kudos
Reply
2 Replies

1,745 Views
igorpadykov
NXP Employee
NXP Employee

Hi

from log:

"cma: CMA: failed to reserve 384 MiB"

seems cma size should be decreased.

Best regards

igor

1,745 Views
尚飞汤
Contributor IV

hi,igorpadykov :

Thank you very much!

0 Kudos
Reply