imx6DL How to make the camera input std PAL by tp2825 to display screen

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6DL How to make the camera input std PAL by tp2825 to display screen

2,463 次查看
lianglou
Contributor II

For the PAL input, the output is non-standard by tp2825。

0 项奖励
回复
5 回复数

2,282 次查看
lianglou
Contributor II

pastedImage_1.png

it can't lock vsync

0 项奖励
回复

2,282 次查看
lianglou
Contributor II

P70926-164430.jpg

refer to the patch https://community.nxp.com/docs/DOC-330441?commentID=41815#comment-41815 ;

experimental result;

how do  even field and odd field combine? 

0 项奖励
回复

2,282 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can refer to the patch https://community.nxp.com/docs/DOC-330441?commentID=41815#comment-41815 .

Have a nice day

Rita

0 项奖励
回复

2,282 次查看
lianglou
Contributor II

P70926-132121.jpg

this is implement by IPU_CSI_CLK_MODE_CCIR656_PROGRESSIVE

0 项奖励
回复

2,282 次查看
lianglou
Contributor II

the output is Y-C Interleaving output mode per 8-bit. field rate is 50Hz.frame rate is 25hz; pclk is 74.25MHz; resolution is 1920X576;pixelformat = V4L2_PIX_FMT_UYVY;  

0 项奖励
回复