imx6D Kernel display flicker

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6D Kernel display flicker

3,090 次查看
jiujinhong
Contributor IV

Hi,

Hardware support 2 LVDS Display, BSP support them adaptively. But one of them flicker in Linux kernel stage. If reboot through reboot cmd(WDOG1), it will not flicker.

I suspect that this is consistence issue which generate by U-boot/Kernel IPU/Clock settings?

BSP:

Linux 4.1.15  (Original BSP, not apply any patch)

U-boot 2015.4 (have applied U-boot patch from https://community.nxp.com/docs/DOC-98109  ).

标签 (4)
0 项奖励
回复
2 回复数

2,876 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jiu

one can check that both lvds clocks are enabled using procedure described in

EB821 LDB Clock Switch Procedure & i.MX6 Asynchronous Clock Switching Guidelines

https://www.nxp.com/docs/en/engineering-bulletin/EB821.pdf 

Also one can check if lvds clock was not used by other module, as for example below

https://community.nxp.com/thread/465848 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,876 次查看
jiujinhong
Contributor IV

Hi Igor,

I have checked both,  there are init_ldb_clocks in  clk-imx6q.c which do you mentioned, and there are no other use LDB clock.

WHY the other display is good without flicker?

0 项奖励
回复