imx6 without linux OS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 without linux OS

2,389 Views
peterc
Contributor I

Is it possible to run a small custom boot application on the imx6, with for example a main loop.

And not a linux distribution as OS. So I have full control over the Firmware that is running.

I would like to use the imx6 in an aviation application. For that reason the firmware running on the device needs to be certified and a LINUX distro is not certified.

So is it possible to boot the imx6 without an thirdparty OS.

Peter

Labels (1)
0 Kudos
Reply
2 Replies

2,084 Views
SergioSolis
NXP Employee
NXP Employee

its bare metal but yes, the SDK is your option:

i.MX6Q|i.MX 6Quad Processors|Quad Core|Freescale

Under "Software Development Tools" >> Software development kits"

0 Kudos
Reply

2,084 Views
saurabh206
Senior Contributor III

Hi,

Peter

You can use imx6_platform_sdk_v1.1.0. for your requirement.

Saurabh

0 Kudos
Reply