imx6 uboot can't get kernel image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 uboot can't get kernel image

7,954件の閲覧回数
teillee
Contributor I

now ,I download the uboot in spi nor and the kernel in emmc ,After uboot parameter set, unable to start the kernel, appear:

  MMC read: dev # 0, block # 2048, count 8192 ... 8192 blocks read: OK

Wrong Image Format for bootm command

ERROR: can't get kernel image

help me!!

uboot Uboot environment variable:

MX6Q SABRELITE U-Boot > print

bootdelay=3

baudrate=115200

ipaddr=192.168.1.103

serverip=_SERVER_IP_ADDR_

netmask=255.255.255.0

loadaddr=0x10800000

rd_loadaddr=0x11000000

netdev=eth0

ethprime=FEC0

ethaddr=00:01:02:03:04:05

uboot=u-boot.bin

kernel=uImage

bootargs_base=setenv bootargs console=ttymxc0,115200

bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p5 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24

bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x2000;bootm

bootcmd=run bootcmd_mmc

stdin=serial

stdout=serial

stderr=serial

ethact=FEC0

bootargs=console=ttymxc0,115200 root=/dev/mmcblk0p5 rootwait rw video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666 video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24

xml burning steps:

   <CMD type="push" body="$ flash_eraseall /dev/mtd0">Erasing Boot partition</CMD>

     <CMD type="push" body="send" file="files/android/u-boot.bin">Sending U-Boot</CMD>

     <CMD type="push" body="$ dd if=$FILE of=/dev/mtd0 bs=512">write U-Boot to SPI-NOR</CMD>

    

     <!-- uncomment below if you store uboot env in your SD card. -->

     <!--

        <CMD type="push" body="$ dd if=/dev/zero of=/dev/mmcblk0 bs=1M count=6">clean up</CMD>

        -->

      <!--

     <CMD type="push" body="send" file="mksdcard-android.sh.tar">Sending partition shell</CMD>

     <CMD type="push" body="$ tar xf $FILE "> Partitioning...</CMD>

     <CMD type="push" body="$ sh mksdcard-android.sh /dev/mmcblk0"> Partitioning...</CMD>

     -->

     <CMD type="push" body="$ ls -l /dev/mmc* ">Formatting sd partition</CMD>

     <CMD type="push" body="send" file="files/android/uImage">Sending kernel uImage</CMD>

     <CMD type="push" body="$ dd if=$FILE of=/dev/mmcblk0p0">write boot.img</CMD>

     <CMD type="push" body="frf">flush the memory.</CMD>

ラベル(1)
タグ(1)
0 件の賞賛
返信
5 返答(返信)

3,292件の閲覧回数
jian_jiang
NXP Employee
NXP Employee

You may use zImage to have a try.

All the best

Jian Jiang

0 件の賞賛
返信

3,292件の閲覧回数
jaymind
Contributor IV

Hello,

I think problem is in below line, u didn't specify

bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 1;mmc read ${loadaddr} 0x800 0x2000;bootm

try to do below and post ur result.....

bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 1:1; load mmc 1:1 10800000 uImage;bootm

and if above not work then try these 2 belows....

bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 1:1;mmc read ${loadaddr} 0x800 0x2000;bootm

bootcmd_mmc=run bootargs_base bootargs_mmc;mmc dev 0:1;mmc read ${loadaddr} 0x800 0x2000;bootm

and make sure about this that your uImage/RFS is in 5th partition of SD card as ur argument showed like this -> root=/dev/mmcblk0p5,so verify it 1st.

post ur results and output.

Hope this will help you

Regards

Jaymin D

0 件の賞賛
返信

3,292件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which OS you run on the board? Linux ? Android?

0 件の賞賛
返信

3,292件の閲覧回数
teillee
Contributor I

linux

0 件の賞賛
返信

3,292件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

seems you selected the Android profile in MFGtool. please select the Linux Profile in MFGtool to write the linux images on your board.

0 件の賞賛
返信