imx6 uart use 9600 baudrate when receiving data issue !

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 uart use 9600 baudrate when receiving data issue !

988 Views
liyu1
Contributor III

Hi ;

        All !

       my platform is imx6q and android kernel version is 3.0.35 .

        I found a bug when  I use uart (9600 baudrate) receiving data form pc,

0412_3.jpg

                                               1 .     android console app

    0412_4.jpg

                                                             2. pc console app

     others baudrate is ok,but 9600 baudrate. sending data also is ok .but receiving . please help me ! thanks !

Labels (2)
0 Kudos
Reply
1 Reply

745 Views
b36401
NXP Employee
NXP Employee

Please make sure that you set the same UART frame options (stopbits, etc) both on PS and i.MX board.

Have a great day,                                                                                                                                                                  

Victor                                                                                                                                                                             

                                                                                                                                                                                   

-----------------------------------------------------------------------------------------------------------------------                                                            

Note: If this post answers your question, please click the Correct Answer button. Thank you!                                                                                       

-----------------------------------------------------------------------------------------------------------------------                                                            

0 Kudos
Reply