imx6 - u-boot binary format

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 - u-boot binary format

1,872件の閲覧回数
Ansari
Contributor IV

Hi,

We are using imx6Q sabresd platform for our development with Linux 3.10.17_1.0.0-GA BSP.


Initially we used L3.0.35_4.** release based u-boot binary.


In L3.0.35_4.** release based binary, the boot able u-boot binary is u-boot.bin.  But in  Linux 3.10.17_1.0.0-GA, the boot able u-boot binary is u-boot-imx.



We would like to know,  the difference between these two formats. Since in Linux 3.10.17_1.0.0-GA BSP also u-boot.bin is generated.


Please suggest us.


 

Thank You,

Regards,

Ansari

0 件の賞賛
返信
1 返信

1,547件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Abdul

please look below for answer

u-boot.bin and u-boot.imx

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信