imx6 spi read/write dma support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 spi read/write dma support

1,196 次查看
ferdi
Contributor I

Hello All:

I would ask if there is a linux3.0.35 based on SPI DMA IMX6Q transfer support, to solve the problem of SPI data overflow, other web pages have a connection with DMA SPI support but can not be opened.

Best regards!

标签 (4)
0 项奖励
回复
1 回复

899 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ferdi

one can develop such driver using existing linux uart driver with sdma support, also

some suggestions are given on

How to do a SPI data transfer using SDMA on iMX6DL

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复