imx6 spi read/write dma support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 spi read/write dma support

1,231 Views
ferdi
Contributor I

Hello All:

I would ask if there is a linux3.0.35 based on SPI DMA IMX6Q transfer support, to solve the problem of SPI data overflow, other web pages have a connection with DMA SPI support but can not be opened.

Best regards!

Labels (4)
0 Kudos
Reply
1 Reply

934 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ferdi

one can develop such driver using existing linux uart driver with sdma support, also

some suggestions are given on

How to do a SPI data transfer using SDMA on iMX6DL

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply