imx6 solo, gpu benchmarking utilities or sample programs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 solo, gpu benchmarking utilities or sample programs

3,817 Views
learner24
Contributor I

Hi,

Is there any benchmarking utility or sample programs which can evaluate the gpu performance . I'm running imx6 solo with 3.14.38 kernel with eglfs support.

Labels (1)
0 Kudos
Reply
3 Replies

3,078 Views
learner24
Contributor I

Thanks for reply.

But, I use linux not andriod. So no support of java to run these apps.

I wanted to test the gpu performance using opengl api's for both 2d and 3d. Currently i use imx6 solo processor which as

vivante gc880 for 3D and supports Open GL ES 2.0 and vivante gc320 for 2D. So, was looking for opengl samples which can help me in evaluating the gpu performance...

0 Kudos
Reply

3,078 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply

3,078 Views
igorpadykov
NXP Employee
NXP Employee

Hi Chaitanya

please look at overview of some benchmarking programs on

Android Graphic UI with GPU Hardware Acceleration | NXP Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply