imx6 solo, gpu benchmarking utilities or sample programs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 solo, gpu benchmarking utilities or sample programs

3,816件の閲覧回数
learner24
Contributor I

Hi,

Is there any benchmarking utility or sample programs which can evaluate the gpu performance . I'm running imx6 solo with 3.14.38 kernel with eglfs support.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,077件の閲覧回数
learner24
Contributor I

Thanks for reply.

But, I use linux not andriod. So no support of java to run these apps.

I wanted to test the gpu performance using opengl api's for both 2d and 3d. Currently i use imx6 solo processor which as

vivante gc880 for 3D and supports Open GL ES 2.0 and vivante gc320 for 2D. So, was looking for opengl samples which can help me in evaluating the gpu performance...

0 件の賞賛
返信

3,077件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信

3,077件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chaitanya

please look at overview of some benchmarking programs on

Android Graphic UI with GPU Hardware Acceleration | NXP Community 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信