imx6 sdma

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,942件の閲覧回数
2548903578
Contributor III

I would like to ask what the <&sdma 3 7 1> parameters mean.

0 件の賞賛
返信
1 解決策
2,935件の閲覧回数
ceggers
Contributor V

This parameter maps:

  • a SDMA event line (3)
  • a peripheral type (7)
  • a SDMA priority (1)

to a peripheral.

Each peripheral has one or two event lines internally connected to the SDMA controller. The SDMA controller has 48 event line inputs at all. In most (all?) i.MX6 reference manuals there is a chapter "3.3 SDMA event mapping" which shows the connection between peripherals and SDMA event lines.
Don't mistake SDMA event lines (48) with SDMA channels (32).

The possible peripheral types are listed in include/linux/platform_data/dma-imx.h:

enum sdma_peripheral_type {
    IMX_DMATYPE_SSI, /* MCU domain SSI */
    IMX_DMATYPE_SSI_SP, /* Shared SSI */
    IMX_DMATYPE_MMC, /* MMC */
    IMX_DMATYPE_SDHC, /* SDHC */
    IMX_DMATYPE_UART, /* MCU domain UART */
    IMX_DMATYPE_UART_SP, /* Shared UART */
    IMX_DMATYPE_FIRI, /* FIRI */
    IMX_DMATYPE_CSPI, /* MCU domain CSPI */
    IMX_DMATYPE_CSPI_SP, /* Shared CSPI */
...
}
So peripheral type 7 is IMX_DMATYPE_CSPI which means SPI over AHB bus.

The SDMA priorities are reverse mapped to reverse mapped to hardware priorities of the SDMA CPU (also include/linux/platform_data/dma-imx.h):

enum imx_dma_prio {
    DMA_PRIO_HIGH = 0,  /* highest possible prio --> hardware prio 3 of 7 */
    DMA_PRIO_MEDIUM = 1, /* medium prio --> hardware prio 2 of 7 */
    DMA_PRIO_LOW = 2   /* lowest prio -> hardware prio 1 of 7 */
};

I would highly appreciate if NXP could provide patches for using preprocessor defines instead of magic numbers in the device tree files. Device tree support preprocessor, but no C style enums.

If you have more questions regarding the SDMA, you can also contact me directly (there is a function in the forum for private messages). I don't scan the forum for new posts everyday...

regards
Christian

元の投稿で解決策を見る

1 返信
2,936件の閲覧回数
ceggers
Contributor V

This parameter maps:

  • a SDMA event line (3)
  • a peripheral type (7)
  • a SDMA priority (1)

to a peripheral.

Each peripheral has one or two event lines internally connected to the SDMA controller. The SDMA controller has 48 event line inputs at all. In most (all?) i.MX6 reference manuals there is a chapter "3.3 SDMA event mapping" which shows the connection between peripherals and SDMA event lines.
Don't mistake SDMA event lines (48) with SDMA channels (32).

The possible peripheral types are listed in include/linux/platform_data/dma-imx.h:

enum sdma_peripheral_type {
    IMX_DMATYPE_SSI, /* MCU domain SSI */
    IMX_DMATYPE_SSI_SP, /* Shared SSI */
    IMX_DMATYPE_MMC, /* MMC */
    IMX_DMATYPE_SDHC, /* SDHC */
    IMX_DMATYPE_UART, /* MCU domain UART */
    IMX_DMATYPE_UART_SP, /* Shared UART */
    IMX_DMATYPE_FIRI, /* FIRI */
    IMX_DMATYPE_CSPI, /* MCU domain CSPI */
    IMX_DMATYPE_CSPI_SP, /* Shared CSPI */
...
}
So peripheral type 7 is IMX_DMATYPE_CSPI which means SPI over AHB bus.

The SDMA priorities are reverse mapped to reverse mapped to hardware priorities of the SDMA CPU (also include/linux/platform_data/dma-imx.h):

enum imx_dma_prio {
    DMA_PRIO_HIGH = 0,  /* highest possible prio --> hardware prio 3 of 7 */
    DMA_PRIO_MEDIUM = 1, /* medium prio --> hardware prio 2 of 7 */
    DMA_PRIO_LOW = 2   /* lowest prio -> hardware prio 1 of 7 */
};

I would highly appreciate if NXP could provide patches for using preprocessor defines instead of magic numbers in the device tree files. Device tree support preprocessor, but no C style enums.

If you have more questions regarding the SDMA, you can also contact me directly (there is a function in the forum for private messages). I don't scan the forum for new posts everyday...

regards
Christian