imx6 sabre smart devices board unable to send a signal when uart2 tx transport text for minicom

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 sabre smart devices board unable to send a signal when uart2 tx transport text for minicom

Jump to solution
2,486 Views
陳冠儒
Contributor IV

hi,all:

why imx6 sabre smart devices board unable to send a signal when uart2 tx  transport text for minicom?

cpu can not send uart2_tx signal  to other side (pc end),but uart5、4、1 can.

Other:

android after boot uart3_tx can send signal  to drive GPS's tx (uart2_tx、uart3_tx set of 3.3V pin,uart1_tx、uart4_tx、uart5_tx set of 1.8V pin).

Might be power problems?

please help me,thanks.

(中譯:為何imx6 sabre smart devices board的uart2_tx不能由minicom 送出文字到另一邊(PC端),也就是cpu的uart2_tx信號完全無信號發出.

          但uart1、4、5卻是可以發出信號.

          其他:

          android 開機後,uart3_tx 卻能送信號去驅動GPS,不過是否是電壓問題呢?uart2_tx、uart3_tx 是設定在 3.3V pin,uart1_tx、uart4_tx、uart5_tx 是設定在1.8V pin)

)

Labels (5)
0 Kudos
Reply
1 Solution
2,288 Views
igorpadykov
NXP Employee
NXP Employee

Hi 陳 冠

I think you can check iomux settings for uart signals, also please

refer to atatched Porting Guide Chapter 3 Registering a New UART Driver.

Also one can try to decrease uart baudrate.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,289 Views
igorpadykov
NXP Employee
NXP Employee

Hi 陳 冠

I think you can check iomux settings for uart signals, also please

refer to atatched Porting Guide Chapter 3 Registering a New UART Driver.

Also one can try to decrease uart baudrate.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,288 Views
陳冠儒
Contributor IV

hi,igorpadykov:

thanks for your help.

I have solved this problem, because I use to repeat the GPIO PIN setting, making it impossible to send data.

thanks!!!

0 Kudos
Reply