imx6 problem with hdmi display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 problem with hdmi display

ソリューションへジャンプ
2,857件の閲覧回数
admin
Specialist II

Hello all,

I am testing the board from Boundary Devices : Nitrogen6X

I am able to boot linux with their kernel. I tried to start a fedora-arm rootfs, and also their

LTIB 2012-08 image.

I can login with the console connector (with serial to usb).

My issue is that I have no display on the hdmi port. I used the bootargs to use hdmi.

I don't know what can be the cause of this issue.

here are some logs :

dmesg :dmesg - Pastebin.com

Xorg :http://pastebin.com/bssXw1pL

gdm/\:0-slave.log : gdm/:0-slave.log - Pastebin.com

xrandr - Pastebin.com

systemd-journal - Pastebin.com


many thanks.

ラベル(3)
0 件の賞賛
返信
1 解決策
2,070件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Looking at the log HDMI does seem to be initialized. Have you tried any other resolution? Sometimes monitors do not support all resolutions or there can be some timing issue with the one you selected...

Vladan

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,071件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

Looking at the log HDMI does seem to be initialized. Have you tried any other resolution? Sometimes monitors do not support all resolutions or there can be some timing issue with the one you selected...

Vladan

0 件の賞賛
返信