imx6 opengl (es) reference code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 opengl (es) reference code

7,035件の閲覧回数
garyyin
Contributor III

imx6q

linux 3.14.28

Have you provided sample code about IMX6 OpenGL (ES) based on bare framebuffer? I need the code based on /dev/fb0 or /dev/fb1, no window backend(X11 and so on).

ラベル(4)
タグ(3)
0 件の賞賛
返信
6 返答(返信)

4,742件の閲覧回数
doerthous
Contributor I

Access denied?

0 件の賞賛
返信

5,706件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Gary,

Samples codes can be found in the GPU SDK package: https://www.nxp.com/webapp/Download?colCode=IMX6_GPU_SDK&location=null&Parent_nodeId=133763715453569... 

Also please check the OpenGL tutorial:

https://community.nxp.com/docs/DOC-134126 

Regards

0 件の賞賛
返信

5,706件の閲覧回数
garyyin
Contributor III

Hi Bio,

Could you provide the related GLES EGL.. libs and gcc toolchain?

Using the imx6 L3.14.28 yocto lib(fb backend) to build, the app throw an error when run.

0 件の賞賛
返信

5,706件の閲覧回数
garyyin
Contributor III

Hi Bio,

Using the sdk you mentioned, I find some function missing:

../common/src/fsl_egl.o: In function `fsl_getNativeDisplay':
fsl_egl.c:(.text+0x18): undefined reference to `fbGetDisplayByIndex'
../common/src/fsl_egl.o: In function `fsl_createwindow':
fsl_egl.c:(.text+0x100): undefined reference to `fbCreateWindow'
collect2: error: ld returned 1 exit status

Do I need some extra lib?

0 件の賞賛
返信

5,706件の閲覧回数
garyyin
Contributor III

I've found the correct libEGL.so. Thanks.

0 件の賞賛
返信

5,092件の閲覧回数
Mav
Contributor I

Hello. I have same problem, trying build OpenGL-fbdev application and have undefined reference to `fbGetDisplayByIndex' and undefined reference to `fbCreateWindow' errors.

It looks like libEGL.so have no fbGetDisplayByIndex and fbCreateWindow functions.

Where did you get correct libEGL.so ?

0 件の賞賛
返信