imx6 linux and android kernel L3.0.35

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 linux and android kernel L3.0.35

3,284件の閲覧回数
jrtigerlee
Contributor III

There are the source code IMX6_JB43_100_ANDROID_SOURCE_BSP and L3.0.35_4.1.0_ER_SOURCE_BSP in Freescale website

They all have its kernel source 3.0.35 with itself patches and different .

Does ltib's embedded linux root filesystems use the same kernel with android's kernel ?

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,432件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Jrtiger,

The android's kernel is Linux 3.0.35 kernel, which is based on Linux BSP L3.0.35_4.1.0 release.

Best Regards

Dan

0 件の賞賛
返信

2,432件の閲覧回数
jrtigerlee
Contributor III

Hi Dan :

Although Android's kernel base on Linux BSP L3.0.35_4.1.0 , but kernel still have lots of patches in android and that patches different from Linux BSP.

So if I build Android's kernel for my Android's system, does this kernel can suitable for my fsl-gnome Linux filesystem that build from LTIB ??

0 件の賞賛
返信

2,432件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Jrtiger,

I think it could be suitable~~Hope this can help you ~~

Best Regards

Dan

0 件の賞賛
返信