Hi,
Lib ipu that was available with im53 doesn't seem to be runable on imx6 in L3.0.35, as it is said in 2012: Re: Is the ipu-lib able to work on iMX6Q?
I wonder if it's really or always the case since you can find ipu lib files in imx-lib package. And functions mxc_ipu_lib_task_init(), mxc_ipu_lib_task_buf_update(),... are present in libipu.so.
Or is it simply not supported by Freescale, but can still work ?
Rgds,
Christophe