imx6 gstreamer h.264 vpu encoding/decoding quality problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 gstreamer h.264 vpu encoding/decoding quality problem

Jump to solution
22,584 Views
sumeetdube
Contributor III

Hi,

We are facing a problem with the quality of h.264 encoding using the imx6q vpu. The video is not clear and there are visible blurring lines on horizontal edges .

We have used following pipeline for h.264 rtp streaming.

1. imx6 board (gstreamer version 0.10)

gst-launch tvsrc ! vpuenc codec=6 ! rtph264pay ! udpsink host=192.168.0.135 port=5000

2. on PC

gst-launch udpsrc port=5000 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, sprop-parameter-sets=(string)\"Z0JAHqaAtD2QAA\\=\\=\\,aM48gAA\\=\", payload=(int)96, ssrc=(uint)1161490911, clock-base=(uint)2476996736, seqnum-base=(uint)7152" ! rtph264depay ! ffdec_h264 ! xvimagesink

Attached is a snapshot of the video saved using the pipeline

gst-launch tvsrc ! vpuenc ! matroskamux ! filesink location=output.mkv sync=false

The video is of very low quality(you can see the fan and cupboard borders are not sharp) and exactly same phenomenon is observed while h.264 rtp streaming .

We are stuck here. Has anybody encountered this problem before ? If so,how to solve it ? We need this solved urgently. Thank you.

Labels (2)
0 Kudos
Reply
1 Solution
17,067 Views
sumeetdube
Contributor III

The problem is solved.

We used this pipeline for display:

gst-launch-1.0 imxv4l2src ! deinterlace mode=1 ! autovideosink

This pipeline to save to file

gst-launch-1.0 imxv4l2src num-buffers=100 ! queue ! deinterlace mode=1 ! imxvpuenc_h264  ! filesink location=out.mkv sync=false

And this to stream

board : gst-launch-1.0 imxv4l2src !  queue ! deinterlace mode=1 ! imxvpuenc_h264  ! rtph264pay ! udpsink host=192.168.0.135 port=5000

PC: H264.sdp file.

I've attached the out.mkv and H264.sdp file . Now there are no lines and the picture is very clear.

View solution in original post

13 Replies
17,067 Views
jamesbone
NXP TechSupport
NXP TechSupport

What version of BSP are you using?,  which board are you using?

0 Kudos
Reply
17,067 Views
sumeetdube
Contributor III

We are using yocto daisy branch . We have made a custom board based on sabrelite which uses tv decoder adv7180 as parallel camera input. 

0 Kudos
Reply
17,067 Views
daiane_angolini
NXP Employee
NXP Employee

In addition to jamesbone​'s questions, please, let me know if you are considering that tvsrc output video frame is interlaced.

0 Kudos
Reply
17,066 Views
sumeetdube
Contributor III

yes we assume the tvsrc output video is interlaced . We used v4l2 ioctls to capture data from adv7180 decoder (set fmt to V4L2_FIELD_INTERLACED) and we could get clear picture. The problem we are facing is in quality of capturing and encoding with gstreamer. Maybe we are missing something in the gstreamer pipeline  which indicates whether interlaced or non-interlaced.

0 Kudos
Reply
17,067 Views
daiane_angolini
NXP Employee
NXP Employee

the picture you shared looks like the same line is being displayed twice.  That's why I asked about interlacing.

Regarding quality. There are several aspects related with quality. When you say quality, what do you mean?

daisy -> there are several "daisy branches". Freescale has released at least 2 releases based on daisy. However, if you are using community source code, and you are still on daisy, I really recomment you to upgrade to fido, because daisy is one year(+) late.

0 Kudos
Reply
17,067 Views
sumeetdube
Contributor III

I dont understand where interlacing comes into play in this gstreamer pipeline .The same pipeline has been used by a lot of developers. By quality i mean the lines that are visible in the image , the image is not sharp or similar to original image. What we want is something closer to the original video that is displayed using the pipeline gst-launch tvsrc ! mfw_v4lsink

0 Kudos
Reply
17,067 Views
daiane_angolini
NXP Employee
NXP Employee

Can you, please generate a movie file with the same bad quality you've been getting with streaming? Something like:

imxv4l2src ->  vpuenc -> muxer -> filesink

Can you, please, use gstreamer 1.0 to test it?

Once you have created the movie, please attach it here

0 Kudos
Reply
17,067 Views
sumeetdube
Contributor III

1.)  For USB-webcam

I did try with a usb webcam and i did not get any lines in the video .

the caps for the webcam were as follows, caps= video/x-raw-yuv, format=(fourcc)YUY2, width= (int)640 , height=(int)480 , interlaced=(boolean)false pixel-aspect-ratio =(fraction)1/1 , framerate =(fraction)30/1

the interlaced parameter  is doing the difference as you said .

2.) For  parallel interface with ADV7180 decoder

I compiled gstreamer-1.0 and worked out the pipeline gst-launch-1.0 imxv4l2src ! autovideosink ,

The lines are more prominent than gst-launch-0.1 tvsrc ! mfw_v4lsink

I will add the clips soon.

Is there any solution to this problem. I know i am doing something wrong with the pipeline, but i cant find out where.

How do i take care of the interlaced parameter in the pipeline.?

0 Kudos
Reply
17,067 Views
daiane_angolini
NXP Employee
NXP Employee

I have never really worked with ADV7180 decoder with gstreamer, so I don't previously know which maybe the parameters to change.

What are the BSP version you are using?

From i.MX Linux® User's Guide , Rev. L3.14.28_1.0.0-ga

7.3.8 Recording the TV-in source

The TV-in source plugin gets video frames from the TV decoder. It is based on the V4l2 capture interface. A command line example is follows:

For gstreamer 1.x use:

gst-launch-1.0 imxv4l2src ! imxv4l2sink

For Gstreamer 010 use:

gst-launch tvsrc ! imxv4l2sink

$GSTL tvsrc num-buffers=100 ! vpuenc ! matroskamux ! filesink location=./output.mkv sync=false

NOTE

The TV decoder is ADV7180. It supports NTSC and PAL TV mode. The output video frame is interlaced, so the sink plugin needs to enable deinterlace. The default value of imxv4l2sink deinterface is True.

0 Kudos
Reply
17,068 Views
sumeetdube
Contributor III

The problem is solved.

We used this pipeline for display:

gst-launch-1.0 imxv4l2src ! deinterlace mode=1 ! autovideosink

This pipeline to save to file

gst-launch-1.0 imxv4l2src num-buffers=100 ! queue ! deinterlace mode=1 ! imxvpuenc_h264  ! filesink location=out.mkv sync=false

And this to stream

board : gst-launch-1.0 imxv4l2src !  queue ! deinterlace mode=1 ! imxvpuenc_h264  ! rtph264pay ! udpsink host=192.168.0.135 port=5000

PC: H264.sdp file.

I've attached the out.mkv and H264.sdp file . Now there are no lines and the picture is very clear.

17,067 Views
世浩李
Contributor II

Hi, would you please show me the command on PC? Thanks!

0 Kudos
Reply
17,069 Views
sumeetdube
Contributor III

Hi we haven't used an interlaced camera with a PC and i even doubt that any of the usb cameras available give interlaced output. So, these pipelines cannot be tested with PC. If you want to use a usb webcam you need to use this pipeline for display :

gst-launch v4l2src device=/dev/video0 ! autovideosink

0 Kudos
Reply
17,067 Views
世浩李
Contributor II

Hi, thanks for your explanation. Actually, in my case, the camera is embedded  on the iMX6 board and I can use the command gst-launch-1.0 imxv4l2src device=/dev/video0 ! vpnenc ! rtph264pay ! udpsink host=192.168.8.101 port=5000 sync=false  to build the pipeline. And I want to use the android mobile phone as the receiver to play the video alive. However, after many attemps, I hava not succeeded still.  I wonder if  you have tried iMX6 board-to-android mobile phone video transmission ? And if so ,would you please show me how to achieve this. Thanks very much!

0 Kudos
Reply