imx6 enet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 enet

1,464 次查看
dongfangxiu
Contributor I

According to i.MX 6 SD Applications Processor reference  manual,

Legacy buffer descriptors are used only in single-ring mode,

that is, when DMAnCFG[DMA_CLASS_EN] are zero.

but I cannot find this register, so when descriptors reach the last one, they cannot warp back, errors happen.

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,284 次查看
igorpadykov
NXP Employee
NXP Employee

Hi dong

for DMA_CLASS_EN description please check

sect.24.5.42 DMA Class Based Configuration (ENETx_DMAnCFG) i.MX6SX Reference Manual

http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SXRM.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,284 次查看
dongfangxiu
Contributor I

Thanks! It comes out my cache has some problem. Another problem is, when I ping my PC with 10000 bytes packets, the link will down sometimes.

0 项奖励
回复