imx6 codecs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 codecs

3,299 Views
kurkinalexandr
Contributor III

Hello. I am trying to build android for CM-FX6.

According to Utilite: Android: Building from source code - Utilite Wiki  I need codecs

Freescale AACP CODEC

Run-time Software
Middleware-Codecs and other Algorithms
IMX6_JB43_110_AACP_CODEC_CODA.

But these codes are absent on the nxp site. Could you help me, where can I take these codecs or replace them by any other codecs?

0 Kudos
Reply
2 Replies

2,803 Views
igorpadykov
NXP Employee
NXP Employee

H Fan

please refer to attached i.MX_6_Series_Android_Codec_Release_Notes.pdf:

Standard codec package is located on common web site.

Other codec packages, like Special codec package (AACP codec, e.t.c.)

contains codecs that are either moderated downloads or separate packages

not part of general distribution. One can contact local marketing for obtaining

them.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,803 Views
danny_lu
Contributor II

Hi igor,

For using AACP special codec package in iMX6Dual lite board of a commercial product, do I need to apply a license from freescale?

Thank you

Danny Lu

0 Kudos
Reply