imx6 camera input resolution?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 camera input resolution?

1,843 Views
kangmw086
Contributor III

I am using the camera in IMX6Q.

The camera resolution setting is used as follows.

1. 1920x1080@30

2. 1440x1080@30

3. 752x582@30

Resolution 1 and 2 work well from camera input to output. But 3 is output as if there is no input from the gstreamer.

Is there a range of resolutions for which IMX6Q can be input?

I thought I only needed to set act_sens_conf and sens_frm_size.

regards!

Labels (3)
0 Kudos
Reply
2 Replies

1,724 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Camera sensors
• Up to three interfaces may be active at once
• Two parallel camera ports (up to 20-bit, up to 240MHz peak1 each).
• MIPI CSI-2 / Parallel port, supporting from 80 Mbps up to 1 Gbps speed per data
lane. The CSI-2 Receiver core can manage one clock lane and up to 4 data lanes.
There are 4 lanes in i.MX 6Dual/6Quad.

0 Kudos
Reply

1,724 Views
kangmw086
Contributor III

Thank you for answer. But that's not the answer I want.

I proceeded to test each one.

However, I set the resolution for 752x582, but the gstreamer is not running. I want to know why.

0 Kudos
Reply