imx6 ar8031 chip

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 ar8031 chip

1,272件の閲覧回数
dngnstjd
Contributor I

Hi, I am using ar8031 ethernet chip on imx6q board.

Link up message is displayed on terminal.

but, does not ping.

I used an oscilloscope to measure the signal levels of RGMII_CLK (ENET_REF_CLK) and RGMII_TXC.

 

RGMII_CLK (ENET_REF_CLK) : 1.4V

RGMII_TXC : 1.2V

I think, The signal level seems too low.

Can I solve this problem by adjusting the impedance on the device tree?

I have already changed the value a few times, but there is no change.

Thank you!!!

0 件の賞賛
返信
1 返信

1,267件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi dngnstjd

 

one can check enet voltage levels using Table 2-9. Gigabit Ethernet Recommendations

IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applic...

and Table 6. Operating Ranges  i.MX 6Dual/6Quad Applications Processors for Consumer Products - Data Sheet

 

Best regards
igor

0 件の賞賛
返信