imx6 android 4.3 build and gstreamer 1.2.x not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 android 4.3 build and gstreamer 1.2.x not working

1,783件の閲覧回数
alokkumar
Contributor III

Hi,

I wanted to test imx6  freescale android box (utilite and nitrogen6x) which has android 4.3 with gstreamer tutorial 3. Though it was working with decodebin pipeline (androidmedia)  and android 4.2.

It was getting following error.

05-10 23:27:05.670 E/BufferQueue( 2462): [SurfaceView] dequeueBuffer: can't dequeue multiple buffers without setting the buffer count

05-10 23:27:05.700 W/GStreamer+bufferpool( 3289): 0:04:10.883391696 0x416518c0 gstbufferpool.c:632:gst_

buffer_pool_set_config:<eglimagebufferpool1> can't change config, we are active
05-10 23:27:05.700 W/GStreamer+bufferpool( 3289): 0:04:10.883543029 0x416518c0 gstbufferpool.c:632:gst_buffer_pool_set_config:<eglimagebufferpool1> can't change config, we are active
05-10 23:27:05.700 E/GStreamer+amcvideodec( 3289): 0:04:10.884113029 0x416518c0 gstamcvideodec.c:806:gst_amc_video_dec_fill_buffer:<amcvideodec-omxfreescalestdvideodecoderavcv3hwbased2> Slice height not set
05-10 23:27:05.700 W/GStreamer+amcvideodec( 3289): 0:04:10.884820362 0x416518c0 gstamcvideodec.c:1314:gst_amc_video_dec_loop:<amcvideodec-omxfreescalestdvideodecoderavcv3hwbased2> error: Invalid sized input buffer
05-10 23:27:05.700 I/tutorial( 3289): Error received from element amcvideodec-omxfreescalestdvideodecoderavcv3hwbased2: Could not configure supporting library.
05-10 23:27:05.700 E/GStreamer+amcvideodec( 3289): 0:04:10.886152696 0x657528c0 gstamcvideodec.c:1683:gst_amc_video_dec_handle_frame:<amcvideodec-omxfreescalestdvideodecoderavcv3hwbased2> Downstream returned not-negotiated
05-10 23:27:05.700 W/GStreamer+qtdemux( 3289): 0:04:10.886591362 0x65752860 qtdemux.c:4404:gst_qtdemux_loop:<qtdemux0> error: streaming stopped, reason not-negotiated

Any suggestions are highly appreciated.

Thanks

Alok

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,230件の閲覧回数
YixingKong
Senior Contributor IV

Alok

We have not got your response yet and will close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信

1,230件の閲覧回数
YixingKong
Senior Contributor IV

Alok

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow resolved the issue, can we close the discussion? If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信