imx6 WebGL performance?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 WebGL performance?

2,065件の閲覧回数
woutervh
Contributor IV

Can somebody explain me what to expect from webgl on a imx6qd board? I have compiled qtwebengine and am running a qt-application in eglfs. When I run a webgl site, it works, but not smooth. Not everything gets rendered too.

However, the CPU load of the qtwebengine process looks rather low (10%-20%) so I have the impression it's not running in software mode. But the performance is that bad, that I cannot imagine that this is the best it can do...

Anybody knows what to expect? Or how I can tweak?

Thanks

タグ(2)
0 件の賞賛
返信
1 返信

1,732件の閲覧回数
mayqueen
Contributor IV

I have same issue, my customers complain for their HTML5 game is very no smooth, we use Chrome on Android 7.1 using imx6Q platform, CPU looks only spend 50% usage, vmalloc=512M, it's not make sense running without smooth, how to improve?

Resolution: 720P

0 件の賞賛
返信