imx6 Solox Galcore device node not getting created

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6 Solox Galcore device node not getting created

1,332 次查看
chintanchoksi
Contributor I

Hello,

We have been working on to run qt 5 on i.MX 6 Solo X board. While running QT application, 

We set following environment variable. 

export QT_QPA_EGLFS_FB=/dev/fb0
export FB_FRAMEBUFFER_0=/dev/fb0
export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1
export QT_QPA_EGLFS_FORCEVSYNC=1
export QT_QPA_PLATFORM=eglfs
We see following error.
/opt/QT_App -platform eglfs
QEglFSVivIntegration will set environment variable FB_MULTI_BUFFER=2 to enable double buffering and vsync.
 If this is not desired, you can override this via: export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1
[     1] Failed to open device: No such file or directory, Try again...
[     2] Failed to open device: No such file or directory, Try again...
[     3] Failed to open device: No such file or directory, Try again...
[     4] Failed to open device: No such file or directory, Try again...
[     5] _OpenDevice(1228): FATAL: Failed to open device, errno=No such file or directory.
[     6] Failed to open device: No such file or directory, Try again...
[     7] Failed to open device: No such file or directory, Try again...
[     8] Failed to open device: No such file or directory, Try again...
[     9] Failed to open device: No such file or directory, Try again...
[    10] _OpenDevice(1228): FATAL: Failed to open device, errno=No such file or directory.
After debugging further, we understand that /dev/galcore node is required which is not being created in our case.
We have enabled following things in kernel config,
CONFIG_DRM_VIVANTE=y
CONFIG_DRM_BRIDGE=y
CONFIG_MXC_IPU=y
CONFIG_MXC_IPU_V3=y
CONFIG_MXC_IPU_V3_PRG=y
CONFIG_MXC_IPU_V3_PRE=y
CONFIG_MXC_GPU_VIV=y
We have also verified that meta-freescale layer has udev entries for galcore device node.
Can anyone point out what can be the issue ?
标签 (3)
0 项奖励
回复
1 回复

1,267 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello chintanchoksi,

pls refer to the document which tell you how to set Environment variables:

How do I set the environment variable XDG_RUNTIME_DIR to '/tmp/runtime-root'? - Help - Chakra's Comm... 

https://wiki.archlinux.org/index.php/environment_variables

Now are using the 4.19.35 BSP?

Regards

0 项奖励
回复