imx6 SPI errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 SPI errors

4,762件の閲覧回数
stasgil
Contributor III

Hi,

We are using a custom board with the imx6qdl processor, with our image based on freescale community bsp for yocto krogoth release.

Kernel version: 4.1.15

Yocto branch: krogoth, 2.0ga

We are extensively using SPI to communicate with several devices(texas istruments microcontrollers) on the SPI bus. Please find our spi-imx.c driver attached.

We are encountering several different errors:

    1) Below are the results of attempting SPI transactions of every length from 0 to 200 16-bit words. The following ranges of message lengths are affected, in bytes:

96-126, 160-190, 224-254, 288-318, 352-382 (decimal).

Transactions with lengths falling in these ranges always fail. This is completely consistent and reproducible.

 

spi_master spi1: I/O Error in DMA RX:60

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:62

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:64

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:66

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:68

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:6a

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:6c

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:6e

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:70

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:72

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:74

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:76

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:78

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:7a

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:7c

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:7e

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:a0

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:a2

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:a4

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:a6

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:a8

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:aa

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:ac

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:ae

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:b0

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:b2

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:b4

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:b6

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:b8

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:ba

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:bc

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:be

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:e0

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:e2

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:e4

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:e6

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:e8

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:ea

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:ec

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:ee

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:f0

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:f2

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:f4

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:f6

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:f8

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:fa

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:fc

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:fe

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:120

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:122

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:124

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:126

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:128

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:12a

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:12c

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:12e

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:130

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:132

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:134

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:136

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:138

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:13a

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:13c

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:13e

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:160

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:162

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:164

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:166

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:168

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:16a

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:16c

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:16e

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:170

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:172

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:174

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:176

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:178

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:17a

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:17c

spi_master spi1: failed to transfer one message from queue

spi_master spi1: I/O Error in DMA RX:17e

spi_master spi1: failed to transfer one message from queue

   2)  Additionally, there is the very rare intermittent fault, that shows up like this:

May 24 16:15:08 imx6dl-ctems kernel: spi_master spi2: I/O Error in RX tail

May 24 16:15:08 imx6dl-ctems kernel: spi_master spi2: failed to transfer one message from queue

May 24 16:15:11 imx6dl-ctems kernel: spi_master spi2: I/O Error in DMA RX:8c

May 24 16:15:11 imx6dl-ctems kernel: spi_master spi2: failed to transfer one message from queue

The second error here is caused by attempting to retry the transaction.

This intermittent fault shows up very roughly once in 100000 transactions.

I have tried the fix from this question : imx6 SPI in DMA mode sometime throws "I/O Error in DMA RX"  but that didn't work

According to this question: SPI DMA support in imx6  and documentation, DMA is not supported in SPI by default. So, how come that all the errors come from the DMA handling code ?

I have not yet tried the patchset from https://community.nxp.com/message/888805?commentID=888805#comment-888805  , but i would like to ask, if there is anywhere i can find an up to date spi-imx.c driver that is compatible with kernel 4.1.15 ?

ラベル(3)
タグ(2)
3 返答(返信)

3,632件の閲覧回数
stasgil
Contributor III

I could not find the root cause, but the I/O Error in DMA RX seem to have been fixed by updating the spi-imx.c driver to a version from the Boundary Devices github page: GitHub - boundarydevices/linux-imx6 at boundary-imx_4.1.15_2.0.0_ga 

Compared to the .c file from krogoth branch, the new one seems to be a lot reliable, with DMA transfer function restructured and workarounds for several silicon ERRATAS added.

I was unable to do anything about the I/O Error in RX tail, so if anyone has any input on this, i would greatly appreciate it :smileyhappy:

Thanks

0 件の賞賛
返信

3,632件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

can you show me your spi setting in the device tree file?

0 件の賞賛
返信

3,632件の閲覧回数
stasgil
Contributor III

Hi, thanks for your reply !

We are using #include "imx6dl.dtsi" in the dts file, and so everything added by that is unchanged. Below are all our SPI related dts changes:

pin control:

pinctrl_ecspi1: ecspi1grp {
fsl,pins = <
MX6QDL_PAD_DISP0_DAT22__ECSPI1_MISO 0x100b1
MX6QDL_PAD_DISP0_DAT21__ECSPI1_MOSI 0x100b1
MX6QDL_PAD_DISP0_DAT20__ECSPI1_SCLK 0x100b1
MX6QDL_PAD_DISP0_DAT23__GPIO5_IO17 0x1b0b0
MX6QDL_PAD_DISP0_DAT15__GPIO5_IO09 0x1b0b0
>;
};

pinctrl_ecspi2: ecspi2grp {
fsl,pins = <
MX6QDL_PAD_DISP0_DAT17__ECSPI2_MISO 0x100b1
MX6QDL_PAD_DISP0_DAT16__ECSPI2_MOSI 0x100b1
MX6QDL_PAD_DISP0_DAT19__ECSPI2_SCLK 0x100b1
MX6QDL_PAD_DISP0_DAT18__GPIO5_IO12 0x1b0b0
MX6QDL_PAD_EIM_D25__GPIO3_IO25 0x1b0b0
>;
};

pinctrl_ecspi3: ecspi3grp {
fsl,pins = <
MX6QDL_PAD_DISP0_DAT2__ECSPI3_MISO 0x100b1
MX6QDL_PAD_DISP0_DAT1__ECSPI3_MOSI 0x100b1
MX6QDL_PAD_DISP0_DAT0__ECSPI3_SCLK 0x100b1
MX6QDL_PAD_DISP0_DAT3__GPIO4_IO24 0x1b0b0

>;
};

SPI devices:

&ecspi1 {
   fsl,spi-num-chipselects = <2>;
   cs-gpios = <&gpio5 17 0>, <&gpio5 9 0>;
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_ecspi1>;
   status = "okay";

   spidev0: spi@0 {
      compatible = "company,SPIdevice";
      reg = <0>;
      spi-max-frequency = <5000000>;
   };

   spidev1: spi@1 {
      compatible = "company,SPIdevice";
      reg = <1>;
      spi-max-frequency = <5000000>;
   };
};

&ecspi2 {
   fsl,spi-num-chipselects = <2>;
   cs-gpios = <&gpio5 12 0>, <&gpio3 25 0>;
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_ecspi2>;
   status = "okay";

   

   spidev2: spi@0 {
      compatible = "company,SPIdevice";
      reg = <0>;
      spi-max-frequency = <5000000>;
   };

   spidev3: spi@1 {
      compatible = "company,SPIdevice";
      reg = <1>;
      spi-max-frequency = <5000000>;
   };
};

&ecspi3 {
   fsl,spi-num-chipselects = <1>;
   cs-gpios = <&gpio4 24 0>;
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_ecspi3>;
   status = "okay";

   spidev4: spi@0 {

      compatible = "company,SPIdevice";
      reg = <0>;
      spi-max-frequency = <5000000>;
   };
};

0 件の賞賛
返信