imx6 SPI data does not seem to be received properly.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 SPI data does not seem to be received properly.

1,278 Views
ktc7270
Contributor II

Hi,

I have imx6q sabresd board.

With the help of the community, I was able to set up the SPI driver.

However, the spi data does not look right.

on the imx6q sabresd board

2.PNG

Is the spi driver not properly configured?

If the settings are wrong, how can I fix them?

Also, is there any C code to read this spi data and save it in file form?


My final goal is to save the spi data I am reading on the imx6sabresd board to a file.

Please help me.

Best regards,

kangta

Labels (3)
0 Kudos
Reply
1 Reply

878 Views
igorpadykov
NXP Employee
NXP Employee

Hi kangta

please check

java - Read received data via /dev/spi* - Stack Overflow 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply