platform: i.mx6Q + SGTL5000
kernel: L3.0.35_4.1.0
produce an audio file only have left channel,(fill all the data of right channel to zero)
stop all of the app, and only play the audio file by aplay,
most of the time, it can work properly,(there are sound only in the left channel), but occasionally, the sound comes from right channel, some times it can return back ,but some times didn't, it will work properly after you reboot system.
we check the LRCLK of I2S of i.mx6 side, the waveform corresponds to the above phenomenon, seems it can exclude the issue of SGTL5000,
we stop all of the app and try to use another audio play app, seems it can exclude the issue of app,
and it can very difficult to reproduce
so is there any bugs of the drivers of SGTL5000? or any other suggestion?
thanks a lot