imx6 JB4.3 kernel GPU driver panic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 JB4.3 kernel GPU driver panic

1,858件の閲覧回数
huyugui
Contributor I

We use imx6d JB4.3 BSP on our custom board.

On music app, I touch down & up on the music list, GPU driver crash sometimes.

 

 

Bellowed  commands are auto test I used:

while true ; do adb shell input touchscreen swipe 330  300 330 550 40;adb shell input touchscreen swipe 330  550 330 300 40 ;done

panic log:

--------------------------

[ 3887.330802] Unable to handle kernel paging request at virtual address befcabb0

[ 3887.338223] pgd = d6ddc000

[ 3887.341092] [befcabb0] *pgd=26d84831, *pte=00000000, *ppte=00000000

[ 3887.348346] Internal error: Oops: 80000007 [#1] PREEMPT SMP

[ 3887.353935] Modules linked in: pateo_sdio wlcore_sdio wl18xx wlcore mac80211 cfg80211 compat gps_drv btwilink st_drv ipod_mfi max21000 mpl3115a2 xf6000ye snd_usb_audio snd_usbmidi_lib snd_rawmidi snd_hwdep pl2303 option usb_wwan usbserial pptp pppopns pppolac pppoe pppox ppp_synctty ppp_mppe ppp_deflate ppp_async bsd_comp ppp_generic slhc asteroid_gt9xx evdev fuse msdos vfat fat galcore

[ 3887.388762] CPU: 0    Not tainted  (3.0.35_ASTEROID-00018-g82adcb2 #1)

[ 3887.395304] PC is at 0xbefcabb0

[ 3887.398491] LR is at gckKERNEL_AddProcessDB+0x2c0/0x354 [galcore]

[ 3887.404589] pc : [<befcabb0>]    lr : [<bf00abac>]    psr: 00030013

[ 3887.404594] sp : d789dbe8  ip : d6b347a0  fp : 40789858

[ 3887.416082] r10: 00000000  r9 : 40789858  r8 : 00000000

[ 3887.421309] r7 : 00000389  r6 : 098967af  r5 : 00000000  r4 : d605b8a0

[ 3887.427838] r3 : cee5cfdc  r2 : 00000000  r1 : 00000000  r0 : 3aa39b5b

[ 3887.434369] Flags: nzcv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

[ 3887.441507] Control: 10c53c7d  Table: 26ddc04a  DAC: 00000015

[ 3887.447254]

[ 3887.447256] SP: 0xd789db68:

[ 3887.451536] db68  0000024c 00000001 0000024c 00000001 00000000 00000001 00000000 00000000

[ 3887.459825] db88  00000000 0000040f 00000007 098967af 00000389 c003cbd4 3aa39b5b 00000000

[ 3887.468112] dba8  00000000 cee5cfdc d605b8a0 00000000 098967af 00000389 00000000 40789858

[ 3887.476399] dbc8  00000000 40789858 d6b347a0 d789dbe8 bf00abac befcabb0 00030013 ffffffff

[ 3887.484687] dbe8  00000000 d602bc40 098967af 00000389 d6c42840 d6c42840 00000000 d6c42840

[ 3887.492973] dc08  00000001 40789858 00000000 bf005300 00000000 00000000 d6c42780 bf009480

[ 3887.501260] dc28  d6c42780 00000000 4080bb38 bf009814 c05ce000 c008ed90 c061380c ffffffff

[ 3887.509547] dc48  c05ce000 00000002 00000000 c008f05c 00000000 c176a4b8 d60ed9c8 c05ce01c

[ 3887.517834]

[ 3887.517836] IP: 0xd6b34720:

[ 3887.522116] 4720  44524148 d6a6f3c0 d6298200 00000355 00001215 1e2c7cc8 0024207f 00010104

[ 3887.530404] 4740  00000000 00000001 00000001 00000001 fffffffe 00000000 00000000 d6008540

[ 3887.538691] 4760  00000005 00000001 00000001 00000001 00000000 00000000 00000000 00000000

[ 3887.546977] 4780  fffb7698 0000012c d6165800 00000000 d6c11320 00000001 00000000 00000000

[ 3887.555263] 47a0  d7924a00 00000000 00000000 00000000 00000000 00000000 d3b97800 d2a76a00

[ 3887.563551] 47c0  00000000 d78e3000 d7be7000 00000000 d78e3e00 00000000 00000000 00000000

[ 3887.571839] 47e0  d6b2f780 00000000 d27b4860 d2fee400 00000840 000001a4 0a272532 00000389

[ 3887.580127] 4800  777159a7 00000161 cee5cc54 00000388 588fc81d 00000161 d6a6f500 d6008420

[ 3887.588414]

[ 3887.588416] R3: 0xcee5cf5c:

[ 3887.592697] cf5c  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.600986] cf7c  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.609273] cf9c  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.617559] cfbc  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.625846] cfdc  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.634132] cffc  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.642419] d01c  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.650705] d03c  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.658992]

[ 3887.658994] R4: 0xd605b820:

[ 3887.663273] b820  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.671560] b840  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.679846] b860  00004e20 d6a6f3c0 c3618722 20f3b74c b051118c 4581c9a2 d10ac020 501750c0

[ 3887.688133] b880  8091ec02 b924c176 06cca050 d2302059 04e8c652 a2094889 34600210 35162227

[ 3887.696421] b8a0  4e52454b d6298200 00000001 d6c42840 d6c42780 d6c45c00 d6c26800 d6298140

[ 3887.704708] b8c0  d60084a0 00000000 d6b347a0 00000000 d6c40ca0 d6008520 00000000 00000000

[ 3887.712995] b8e0  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.721281] b900  00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000

[ 3887.729571] Process SurfaceFlinger (pid: 1255, stack limit = 0xd789c2f0)

[ 3887.736275] Stack: (0xd789dbe8 to 0xd789e000)

[ 3887.740636] dbe0:                   00000000 d602bc40 098967af 00000389 d6c42840 d6c42840

[ 3887.748819] dc00: 00000000 d6c42840 00000001 40789858 00000000 bf005300 00000000 00000000

[ 3887.757002] dc20: d6c42780 bf009480 d6c42780 00000000 4080bb38 bf009814 c05ce000 c008ed90

[ 3887.765185] dc40: c061380c ffffffff c05ce000 00000002 00000000 c008f05c 00000000 c176a4b8

[ 3887.773367] dc60: d60ed9c8 c05ce01c 00000000 d789c000 c05ec0c8 c008f080 c176a060 d60ed820

[ 3887.781550] dc80: d789dd34 c04589a0 00000000 00000000 00000000 c0036060 00000000 c0069d58

[ 3887.789732] dca0: 00000000 00000000 000003f1 d789dde8 00000002 00000000 00000000 00000000

[ 3887.797915] dcc0: 00000000 00000000 d602bc40 ffffffff c0036060 00000000 d6008cc0 00000000

[ 3887.806097] dce0: 00000000 c0036060 00000000 c004c6f4 c0645708 00000000 00000000 00000000

[ 3887.814279] dd00: 00000000 00000001 00000001 00000001 00000000 00000001 00000000 d6008cc0

[ 3887.822462] dd20: 00000000 000007df 00000000 00000000 00000000 00000000 00000001 00000018

[ 3887.830644] dd40: 00000000 d7827000 d7827058 c032bd68 d789ddbc 00000000 00000000 d0299780

[ 3887.838827] dd60: d41b2780 c03d3654 00000000 00000000 d6b2f7a0 bf002aa8 d6a6f500 00000004

[ 3887.847009] dd80: d6089000 bf007e94 d6b347a0 d789de40 d6c42780 d605b8a0 00000000 00000001

[ 3887.855192] dda0: d789c000 00000000 40789858 bf008998 00000000 00000499 c0037eb8 fffffff5

[ 3887.863374] ddc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000499 00000000

[ 3887.871557] dde0: d41b2780 d789deec 00000018 d6d44e60 c0121e38 c0121e7c 00000104 d789c000

[ 3887.879740] de00: d6c26800 d789c000 d785cd20 00007530 c003d184 d789c000 00000000 bf001a40

[ 3887.887922] de20: 405697a0 00000000 000000a8 00000000 405697a0 00000000 000000a8 00000000

[ 3887.896105] de40: 00000013 00000002 00000000 407898a0 4078a940 00000000 0000000a 20000100

[ 3887.904287] de60: 00000004 00000000 4080bb38 00000000 40789858 00000000 00000000 00000000

[ 3887.912470] de80: 40f93a20 4002f008 00000000 00000000 00000000 00000001 4002f008 406e657d

[ 3887.920652] dea0: 00000001 40569968 00000131 00000000 00000400 00000258 00000000 00000200

[ 3887.928835] dec0: ffffff5c 400cc605 ffffff5c 400cc605 00000400 00000258 405f4344 00000000

[ 3887.937017] dee0: 00000002 00000001 d6cc3328 40569760 d606dc60 0000000e c003d184 d789c000

[ 3887.945200] df00: 00000000 c00fc7ac 00000000 d6224000 d62241c4 00000000 00000001 c01d7684

[ 3887.953382] df20: 00000000 00000001 00000001 00000000 00000022 c063940c c05d2200 c00ae6cc

[ 3887.961565] df40: 00000081 fffffff7 0000833e c05d2200 c05d224c d6182ca0 00000022 00000000

[ 3887.969747] df60: d789c000 d606dc60 40569760 00007530 0000000e c003d184 d789c000 00000000

[ 3887.977930] df80: 40789858 c00fccb0 00000022 00000001 c05e4cd0 00002710 00007530 405f4d80

[ 3887.986113] dfa0: 00000036 c003d000 00002710 00007530 0000000e 00007530 40569760 40569748

[ 3887.994296] dfc0: 00002710 00007530 405f4d80 00000036 4080bb88 401601f4 4080bac8 40789858

[ 3888.002479] dfe0: 00000000 40569738 40140ab7 40130324 60030010 0000000e 00000000 00000000

[ 3888.010716] [<bf00abac>] (gckKERNEL_AddProcessDB+0x2c0/0x354 [galcore]) from [<bf005300>] (gckOS_Broadcast+0x74/0xe8 [galcore])

[ 3888.022238] [<bf005300>] (gckOS_Broadcast+0x74/0xe8 [galcore]) from [<bf009480>] (gckCOMMAND_EnterCommit+0x3c/0xa8 [galcore])

[ 3888.033586] [<bf009480>] (gckCOMMAND_EnterCommit+0x3c/0xa8 [galcore]) from [<bf009814>] (gckCOMMAND_Commit+0x6c/0x9f0 [galcore])

[ 3888.045193] [<bf009814>] (gckCOMMAND_Commit+0x6c/0x9f0 [galcore]) from [<bf008998>] (gckKERNEL_Dispatch+0xa74/0x1178 [galcore])

[ 3888.056706] [<bf008998>] (gckKERNEL_Dispatch+0xa74/0x1178 [galcore]) from [<bf001a40>] (drv_ioctl+0x110/0x260 [galcore])

[ 3888.067598] [<bf001a40>] (drv_ioctl+0x110/0x260 [galcore]) from [<c00fc7ac>] (do_vfs_ioctl+0x80/0x54c)

[ 3888.076913] [<c00fc7ac>] (do_vfs_ioctl+0x80/0x54c) from [<c00fccb0>] (sys_ioctl+0x38/0x5c)

[ 3888.085191] [<c00fccb0>] (sys_ioctl+0x38/0x5c) from [<c003d000>] (ret_fast_syscall+0x0/0x30)

[ 3888.093636] Code: bad PC value

[ 3888.096916] imx-esai imx-esai.0: Resetting ESAI!

[ 3888.114020] ---[ end trace 1485f45e9ca71ddf ]---

[ 3888.118986] Kernel panic - not syncing: Fatal exception

[ 3888.124311] [<c0043c90>] (unwind_backtrace+0x0/0xf8) from [<c0454cc0>] (panic+0x78/0x194)

[ 3888.132766] [<c0454cc0>] (panic+0x78/0x194) from [<c0040b30>] (die+0x218/0x284)

[ 3888.140166] [<c0040b30>] (die+0x218/0x284) from [<c0454acc>] (__do_kernel_fault.part.3+0x54/0x74)

[ 3888.149117] [<c0454acc>] (__do_kernel_fault.part.3+0x54/0x74) from [<c00478b8>] (do_page_fault+0x2b4/0x31c)

[ 3888.158943] [<c00478b8>] (do_page_fault+0x2b4/0x31c) from [<c00374ac>] (do_PrefetchAbort+0x34/0x9c)

[ 3888.168103] [<c00374ac>] (do_PrefetchAbort+0x34/0x9c) from [<c003cbd4>] (__pabt_svc+0x74/0xc0)

[ 3888.176785] Exception stack(0xd789dba0 to 0xd789dbe8)

[ 3888.181858] imx-esai imx-esai.0: TX#0 Not enough data in ALSA buffer (24 frames)

[ 3888.189335] dba0: 3aa39b5b 00000000 00000000 cee5cfdc d605b8a0 00000000 098967af 00000389

[ 3888.197584] dbc0: 00000000 40789858 00000000 40789858 d6b347a0 d789dbe8 bf00abac befcabb0

[ 3888.205806] dbe0: 00030013 ffffffff

[ 3888.209332] [<c003cbd4>] (__pabt_svc+0x74/0xc0) from [<befcabb0>] (0xbefcabb0)

[ 3888.216593] CPU1: stopping

[ 3888.219318] [<c0043c90>] (unwind_backtrace+0x0/0xf8) from [<c00373a8>] (do_IPI+0x1d4/0x208)

[ 3888.227679] [<c00373a8>] (do_IPI+0x1d4/0x208) from [<c003cce8>] (__irq_usr+0x48/0xe0)

[ 3888.235513] Exception stack(0xd7fb9fb0 to 0xd7fb9ff8)

[ 3888.240569] 9fa0:                                     40629260 4062925f 5a5f006a 0000005f

[ 3888.248752] 9fc0: 400eaed8 406249d8 00000089 4062925e 40624148 40627b98 bed31578 4063a810

[ 3888.256933] 9fe0: 0000005f bed31488 400d2fe7 400d7078 60070030 ffffffff

[ 3888.263554] Rebooting in 20 seconds..

Original Attachment has been moved to: AudioUI-(2).apk.zip

ラベル(5)
0 件の賞賛
返信
1 返信

1,444件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

The error it is just happening using your  APK, that you are sharing? or using the Android based tools it is also happening this issue?. Have you try your APK in a freescale boarD? like the SABRE SDB?

0 件の賞賛
返信