imx6 DualLite internal boot sequence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 DualLite internal boot sequence

1,467件の閲覧回数
harshakumar
Contributor II

Hi,

ln imx6 DualLite processor internal boot mode is selected and boot straps (eFUSE) are not set, in this case what is the boot flow ? and which boot mode has high priority of boot in above case (usdhc1 or usdhc2) ?

Thanks,

Harsha

ラベル(1)
0 件の賞賛
返信
1 返信

1,340件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Harsha,

For fuse blow one can look below

 

Q&A: How to program i.MX6 eFUSE?

If one selected boot from fuses, this fuse selection can no be changed, since fuses are one time programmable.

https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX6DQ6SDLSRM&appType=moderatedWith... 

Table. Boot MODE Pin Settings

 

Fuses select just boot options, after boot all modules remain fully

functional, that is :SD card will support SD3 and EMMC will support SD4.

Regards

0 件の賞賛
返信