imx6 DualLite internal boot sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 DualLite internal boot sequence

1,211 Views
harshakumar
Contributor II

Hi,

ln imx6 DualLite processor internal boot mode is selected and boot straps (eFUSE) are not set, in this case what is the boot flow ? and which boot mode has high priority of boot in above case (usdhc1 or usdhc2) ?

Thanks,

Harsha

Labels (1)
0 Kudos
Reply
1 Reply

1,084 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Harsha,

For fuse blow one can look below

 

Q&A: How to program i.MX6 eFUSE?

If one selected boot from fuses, this fuse selection can no be changed, since fuses are one time programmable.

https://www.nxp.com/webapp/sps/download/mod_download.jsp?colCode=IMX6DQ6SDLSRM&appType=moderatedWith... 

Table. Boot MODE Pin Settings

 

Fuses select just boot options, after boot all modules remain fully

functional, that is :SD card will support SD3 and EMMC will support SD4.

Regards

0 Kudos
Reply