imx6 BAR0 limit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 BAR0 limit

1,231件の閲覧回数
bluesky507
Contributor I

Hello

I checked pci driver sources provided for IMX.6 CPU. It seems that ddr memory window reserved for root complex is limited to 16M. I need at least 256M for BAR0 in my application. Is it possible to patch the driver to support such memory size?

0 件の賞賛
返信
1 返信

1,134件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Only 16 MB address range is available for PCIe in i.MX6 system memory map.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信