imx6 BAR0 limit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 BAR0 limit

507 Views
bluesky507
Contributor I

Hello

I checked pci driver sources provided for IMX.6 CPU. It seems that ddr memory window reserved for root complex is limited to 16M. I need at least 256M for BAR0 in my application. Is it possible to patch the driver to support such memory size?

0 Kudos
Reply
1 Reply

410 Views
Yuri
NXP Employee
NXP Employee

Hello,

Only 16 MB address range is available for PCIe in i.MX6 system memory map.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply