imx53, opengles2 & libglx?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx53, opengles2 & libglx?

2,819 次查看
woutervh
Contributor IV

I want to have libglx on my imx53-platform. However, it drops back to software mode?

[1424995.145] (II) AIGLX: Screen 0 is not DRI2 capable
[1424995.145] (EE) AIGLX: reverting to software rendering
[1424995.240] (II) AIGLX: Loaded and initialized swrast
[1424995.240] (II) GLX: Initialized DRISWRAST GL provider for screen 0

Can I make it run in hardware? So it uses the available opengles2 engine?

(I'm not very familiar with opengl/glx stuff, so don't shoot if it's a silly question ;-))

标签 (4)
5 回复数

2,581 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Wouter

for hardware opengl one can try latest i.MX53 NXP official bsp (it is L2.6.35), please use

attached Linux Manual Chapter 16 Graphics Processing Unit (GPU).

Linux 2.6.35 Source Code Files and documentation (REV L2.6.35)
https://www.nxp.com/webapp/Download?colCode=L2.6.35_1.1.0_ER_SOURCE&appType=license&location...

Submit i.MX53 & i.MX28 Linux kernel patches 

Software was not developed for newer kernels so hardware opengl support may be absent.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,581 次查看
woutervh
Contributor IV

Thank you, 

but the build I use is based on version 2.6.35 11.09.01...

I only want to know if it's possible to make GLX use opengles2 provisioning?

0 项奖励
回复

2,581 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Wouter

there is no ubuntu support and Linux Manual describes all what

is supported in release, for X11 one can refer to
Chapter 17 X Windows Acceleration Linux Manual. May be useful to look on

Bug #1002818 “Hardware accelerated 3D support is unavailable on ...” : Bugs : Linaro Ubuntu 

Best regards
igor

0 项奖励
回复

2,581 次查看
woutervh
Contributor IV

Yes, but it's not ubuntu.

It's yocto Fido. And yocto fido gets all MM-packages of 2.6.35 / 11.09.01 as far as I can tell

0 项奖励
回复

2,581 次查看
igorpadykov
NXP Employee
NXP Employee

for yocto one can look at

Public images - fsl-community-bsp/master/ 

0 项奖励
回复