imx53 mfw_isink vssconfig configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx53 mfw_isink vssconfig configuration

Jump to solution
3,043 Views
janiscoders
Contributor III

Hi, we are developing our custom board based on imx53 QSB using Yocto building system. Recently tried to use mfw_isink element, which allows to display multiple videos

on the same display at the same time. I am no specialist in Linux graphic system (framebuffer, x11), so it would be great if someone explained me these issues:

1) When I boot board with lvds screen without any configurations, I have everything as expected - the linux boot information with login prompt can bee seen on display.

If I play video or live camera using mfw_v4lsink, everything plaus fine fullscreen and goes back to previous display.

BUT playing videos with mfw_isink doesn't work out of the box. I read somewhere that /usr/share/vssconfig has to be changed and set fb to 0.

What really is this vssconfig file? Is there a documentation available? What does this command (fb) do and why it is set to 1 by default?

2) The multimedia documentation says that I have to set this env variable (export VSALPHA=1). I don't really understand the purpose of it and is it really needed?

3) If I play anything with mfw_isink then at first time video is playing, but everything is blinking in many colours. After that the display doesn't go back to previous

state like it does for mfw_v4lsink (i.e. the login screen isn't displayed anymore). It isn't refreshed in reality, because I can see the little blinking underscore only.

Playing video again it plays without colour blinking.

4) After a while video playing using mfw_v4lsink doesn't work anymore (it works, but nothing is being displayed. Probably something has timed out or somthing).

Anyway mfw_isink still shows video at this state.

It would be great if someone answered at least to some of these questions. Thatnk you :smileyhappy: (it would be great, getting isink to work, because it is really powerful)

Labels (4)
0 Kudos
Reply
1 Solution
2,069 Views
janiscoders
Contributor III

I think I found answers to my questions by myself.

1) Seems like /usr/share/vssconfig file is used by mfw_isink plugin and is cached (if you change something, then /dev/shm/ must be cleared [or reboot] to enable new configurations ).

Yocto dora branch at this time doesn't change vssconfig fb_num value, which by default is 1 - and that does nothing for master screen.

Seems like mfw_isink on exit sets framebuffer to sleep, that’s why screen doesn't go to previous state, like it is with mfw_v4lsink (this is only relevant when fb_num is set to 0) Read further....

In reality the fb_num must be set to value 2, then mfw_isink doesn't set framebuffer to sleep and everything goes back to normal.

2) If fb_num is set to correct value: 2, then this environment exporting is needed to see mfw_isink output. I did the export in /etc/profiles, so it would be global.

3) Previously I changed fb_num value to 0, which I think overlapped with terminal fb and thats why there was flickering conflict. If fb_num is set to 2, then there is no flickering.

4) Linux framebuffer goes to sleep after 10 minutes (this is the default), that’s why screen disappears. To disable/change this you must pass kernel parameter or write commands to /dev/tty1.

More info here:

www.armadeus.com/wiki/index.php?title=FrameBuffer

Change Linux console screen blanking behavior - Super User

View solution in original post

0 Kudos
Reply
4 Replies
2,070 Views
janiscoders
Contributor III

I think I found answers to my questions by myself.

1) Seems like /usr/share/vssconfig file is used by mfw_isink plugin and is cached (if you change something, then /dev/shm/ must be cleared [or reboot] to enable new configurations ).

Yocto dora branch at this time doesn't change vssconfig fb_num value, which by default is 1 - and that does nothing for master screen.

Seems like mfw_isink on exit sets framebuffer to sleep, that’s why screen doesn't go to previous state, like it is with mfw_v4lsink (this is only relevant when fb_num is set to 0) Read further....

In reality the fb_num must be set to value 2, then mfw_isink doesn't set framebuffer to sleep and everything goes back to normal.

2) If fb_num is set to correct value: 2, then this environment exporting is needed to see mfw_isink output. I did the export in /etc/profiles, so it would be global.

3) Previously I changed fb_num value to 0, which I think overlapped with terminal fb and thats why there was flickering conflict. If fb_num is set to 2, then there is no flickering.

4) Linux framebuffer goes to sleep after 10 minutes (this is the default), that’s why screen disappears. To disable/change this you must pass kernel parameter or write commands to /dev/tty1.

More info here:

www.armadeus.com/wiki/index.php?title=FrameBuffer

Change Linux console screen blanking behavior - Super User

0 Kudos
Reply
2,069 Views
LeonardoSandova
Specialist I

rogeriopimentel, could you please check the above points and make any comments if necessary.

Janis, it looks to me that you may have to create a patch to change the vssconfig value. Can you share these results in the same thread you started on the meta-freescale list?

0 Kudos
Reply
2,069 Views
LeonardoSandova
Specialist I

Could you send this to the meta-freescale list? There were some issues on iMX6 regarding isink, but not related to the ones above. Please post logs on each issue you faced.

Leo

0 Kudos
Reply
2,069 Views
janiscoders
Contributor III

I fixed some of my first problems (not the ones described here) using meta-freescale and read the old mail archive, where people had  problems with isink and they were a little related, but didn't answer everything.
What I am really interested in - is this vssconfig file. What are the configuration possibilities and how they are related? Not really sure if this is Yocto related, thats why I am asking here.

Only maybe the 4th question could be asked in meta-freescale.

0 Kudos
Reply