Hi. We have created our own board based on SMD and LOCO and added camera ov5640.
I am using kernel patches-imx-2.6.35_11.09.0 from github. Filesystem is Ubuntu armhf.
Camera driver is loaded with all dependencies and I can record videos with tools like avconv, ffmpeg. But everything hangs when using mencoder of gstreamer, and in kernel log I can see calling this all the time:
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0485619
case VIDIOC_ENUMSTD
What I really want is to get better video cam resolution and it doesn really get better changing ffmpeg parameters. As I've seen others on IMX community use gstreamer, but I can't get it working with parameter "mfw_v4lsrc".
Should I install Freescale provided .deb packages to get this working? But they all are armel, but I have armhf system.
I've tried to change capture mode in driver and it changes to 1280x720, but what is the v2f value, which still stays low?
KERNEL LOG: End of mxc_v4l_open: v2f pix widthxheight 288 x 352
Because it looks like ffmpeg is using this resolution.
解決済! 解決策の投稿を見る。
Yes, it is better to install all the deb packages that Freescale provided.
Yes, it is better to install all the deb packages that Freescale provided.